Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Clarification on High-Temperature Water Extraction Issue
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 332 subscribers
  • Views 812 views
  • Users 0 members are here
  • industrial
  • vacuum truck
  • heat dissipation
  • cool
  • heat transfer
  • chiller
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Clarification on High-Temperature Water Extraction Issue

Maral
Maral over 1 year ago

Hi Everyone, I wanted to follow up and clarify the situation I previously described regarding the challenges we're facing with water management at a thermal power plant. The Core Problem: Fractured Water Tunnels: We've identified that the water transport tunnels from the thermal power plant have fractures. This is causing hot water to leak into an underground concrete tank, which is situated above the heat line. Temperature Escalation: Over time, this water, which starts at temperatures close to 100°C, cools down slightly during transfer, but it still maintains a temperature of about 80°C when it reaches the tank. The tank itself has a small hole, which prevents the water from cooling off naturally and instead allows it to retain, or even gradually increase, its temperature. Operational Challenge: Vacuum Truck Limitations: Our current vacuum trucks aren’t equipped to handle such high temperatures. Vacuuming hot water means also vacuuming hot air, which leads to technical failures in the trucks. As a workaround, we've been adding cold water to bring down the temperature before vacuuming, but this isn’t efficient. The water left behind in the tank heats up again by the time the truck returns, leading to water waste and increased operational costs. Proposed Solutions: Cooling Before Vacuuming: Implementing a heat transfer system or portable chillers to cool the water quickly. Using collapsible tanks to store hot water temporarily, though this solution isn’t ideal in urgent situations. Exploring the use of non-toxic chemical cooling agents. Vacuuming While Hot: Considering a switch to vacuum trucks that can withstand temperatures above 80°C. Adding insulation to the vacuum lines to manage heat transfer better. Using specialized pumps for hot liquids, separate from the main vacuum system. Additional Insights Needed: I'm seeking further insights to refine these solutions or explore new ones. Specifically: Temporary Cooling Methods: Any field-tested cooling methods that can be deployed quickly and effectively. High-Temperature Vacuum Systems: Recommendations on vacuum systems or pumps designed for handling high-temperature liquids. Emergency Solutions: Any innovative or unconventional approaches that could be effective in urgent scenarios. Thanks again to everyone who has already provided feedback. I hope this clarification helps, and I’m eager to hear any additional advice you might have!

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 1 year ago in reply to aswinvenu +1
    See my reply in your original thread. MK
Parents
  • aswinvenu
    0 aswinvenu over 1 year ago

    The primary source of this issue is the cracks/Fractures in the water tunnel.Fixing that will solve this issue! Right?

    May be you can insert copper tubes inside the tank and connect it to a radiator. Very similar to a water cooler. You can pump water through the tubes to regulate the temperature. In this case this water is not in contact with the hot water. So It wont contaminate.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • aswinvenu
    0 aswinvenu over 1 year ago

    The primary source of this issue is the cracks/Fractures in the water tunnel.Fixing that will solve this issue! Right?

    May be you can insert copper tubes inside the tank and connect it to a radiator. Very similar to a water cooler. You can pump water through the tubes to regulate the temperature. In this case this water is not in contact with the hot water. So It wont contaminate.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • michaelkellett
    0 michaelkellett over 1 year ago in reply to aswinvenu

    See my reply in your original thread.

    MK