Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum OPENUPS Configuring
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 333 subscribers
  • Views 1074 views
  • Users 0 members are here
  • ask_an_expert
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

OPENUPS Configuring

Jasroop92
Jasroop92 over 1 year ago

Hi, we need help with Configuring OpenUPS.

We have an internal battery, plus 2 mainline connections coming in. 1 is Type C and 1 is an external battery plate.

The issue we are having is configuring the OpenUPS board.

When the power is coming through the type c or external battery plate, is should power our unit plus charge the internal battery.

When there is no external power input it should run on the internal battery.

The issue we face is when we are being powered by an external source it is not powering the internal battery at the desired voltage, it is charging at 13.8V when it should be between 14.2V and 14.7V.

The second issue is that we have a power switch attached to the openUPS which will only turn on when the power button is held for 5 seconds or more. Ideally, we would like this to be around 1 second.

Finally, if you have a better understanding of OpenUPS then it would be great if we could understand how to configure it better.

I'd be happy to go into more detail on how exactly our system is setup but anyone with OPENUPS expertise would be greatly appreciated.

Thanks in advance!

  • Sign in to reply
  • Cancel

Top Replies

  • anniel747
    anniel747 over 1 year ago +1
    Deleted
Parents
  • anniel747
    anniel747 over 1 year ago
    This reply was deleted.
    • Cancel
    • Cancel
Reply
  • anniel747
    anniel747 over 1 year ago
    This reply was deleted.
    • Cancel
    • Cancel
Children
  • Jasroop92
    0 Jasroop92 over 1 year ago in reply to anniel747

    Thanks for this. I've already been through the documentation but still can't work this out. Ideally, I need to speak with someone who is well-versed in using the OPENUPS with all of the different parameters.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • JWx
    0 JWx over 1 year ago in reply to Jasroop92

    AFAIK 13.8V is the correct voltage for standby battery use:

    from random datasheet:

    Cycle Use Inital Charging Current less than 2.55A.Voltage 14.4V ~ 15.0V Temp. Coefficient -30mV/°C
    Standby Use No limit on Initial Charging Current Voltage 13.5V ~ 13.8V Temp. Coefficient -20mV/°C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer