Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Issue with Receiving Structured Data via UART Callback on STM32
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 336 subscribers
  • Views 2698 views
  • Users 0 members are here
  • usart
  • sensors
  • stm32f407ig
  • stm32
  • uart
  • electronics
  • stm32f4discovery
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Issue with Receiving Structured Data via UART Callback on STM32

pooja_14
pooja_14 over 1 year ago

Hello,

I'm working with two different STM32 microcontrollers:

  • Sender: STM32F4CCUx
  • Receiver: STM32F4VET6

I am sending a packet (which is a structure of size 4) from the sender to the receiver using UART, with both microcontrollers utilizing the UART callback function for transmission and reception.

Here is the process I’m following:

  1. The sender sends a packet using HAL_UART_Transmit_IT.
  2. The receiver is configured with HAL_UART_Receive_IT.
  3. Both microcontrollers handle data in their respective callback functions.

However, on the receiving side, the data is either jumbled or incorrect.

Details:

  • The packet is a structured type with multiple fields.
  • I’ve ensured that the baud rate and UART configurations match on both microcontrollers.
  • The callback functions seem to be triggering correctly.
  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 1 year ago +1 suggested
    There are a lot of useful examples (google ' STM32 UART interrupt receive example '). It would be best to start with one of those examples, so that you have known working code. Some of those examples…
Parents
  • shabaz
    0 shabaz over 1 year ago

    There are a lot of useful examples (google 'STM32 UART interrupt receive example').

    It would be best to start with one of those examples, so that you have known working code. 

    Some of those examples are precisely for the situation where the length of the received data is unknown, i.e. you will be able to view data in a buffer and process it once your code determines a complete set of data has arrived (it is up to your code to decide on that).

    Start with one of the examples, and that will confirm to you that the sender side data is successfully being received correctly. Without that, it's like a stab in the dark.

    Then, code your algorithm to determine when the received data is sufficient to process as a complete message.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 1 year ago

    There are a lot of useful examples (google 'STM32 UART interrupt receive example').

    It would be best to start with one of those examples, so that you have known working code. 

    Some of those examples are precisely for the situation where the length of the received data is unknown, i.e. you will be able to view data in a buffer and process it once your code determines a complete set of data has arrived (it is up to your code to decide on that).

    Start with one of the examples, and that will confirm to you that the sender side data is successfully being received correctly. Without that, it's like a stab in the dark.

    Then, code your algorithm to determine when the received data is sufficient to process as a complete message.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer