Hello I want to build a non-contact pH meter. Is this possible? I would like to get detailed information and help on this subject.
Be sure to click 'more' and select 'suggest as answer'!
If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!
Hello I want to build a non-contact pH meter. Is this possible? I would like to get detailed information and help on this subject.
WHY do you want non contact and will inaccurate reading be acceptable
He doesn't want to have to clean the pH electrodes.
An ultrasonic cleaner is quite simple and straightforward to use and your lab should already have one and buffer solution. I already answer this question in private:
24 Dec 2024
Actually, I'm wondering if a normal pH sensor probe can be cleaned in an ultrasonic cleaner.
Thank you very much. So, what temperature should it be? How many kHz should the liquid inside be? Is tap water acceptable as a cleaning fluid or what kind of liquid should be used?
Thank you very much, I have a few more questions for you. I'm sorry, I'm taking your time. I'm testing an oily and sticky sample, cake cream, so I use it with a probe test 15 times a day.
pastry cream pH range is 7.0 to 5.0, milk, egg, sugar, starch are used, margarine, vanillin, liquid cake whipped cream, these are:
I would use warm 4.01 pH buffer solution as a start and see if there is specific residual contaminants.
So, would it be a problem if we drop liquid detergent into tap water and clean it with an ultrasonic cleaner?
Unfortunately, this system will not be used in the laboratory and pastry cream tests will be performed 20 times a day.
Your production line has no QC lab? The QUANTOFIX Relax can run on 6 AA batteries and it can perform 50 tests per hour.
Your production line has no QC lab? The QUANTOFIX Relax can run on 6 AA batteries and it can perform 50 tests per hour.