Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum How does 569 relate to 5.6pF on an MLCC through hole capacitor, I understand 101 or 104 but why 569?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 335 subscribers
  • Views 2093 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

How does 569 relate to 5.6pF on an MLCC through hole capacitor, I understand 101 or 104 but why 569?

davebullockmbe
davebullockmbe over 1 year ago

Hi I just received what purport to be some through hole 5.6pF MLCC's marked 569, how does this relate to the value?

I understand MLCC's marked 101, 102, 473 as the last number is the multiplier (how many zeroes) but xx9?

Whilst an internet can decipher the value it offers no explanation of the value numbering origin for such low value MLCC's

Please explain.

Thanks

Dave

  • Sign in to reply
  • Cancel

Top Replies

  • davebullockmbe
    davebullockmbe over 1 year ago in reply to michaelkellett +3
    Ha! Mystery solved...the xx9 (9) means there is NO multiplier and infers that the value is BELOW 10pF. I just found this chart (below) Once the value increases above 9.1pF the familiar 100 appears…
  • anniel747
    anniel747 over 1 year ago in reply to davebullockmbe +2 verified
    davebullockmbe Capacitance Code (pF): Two significant digits and number of zeros. Use 9 for 1.0 – 9.9 pF. Use 8 for 0.5 – .99 pF. ex. 2.2 pF = 229 ex. 0.5 pF = 508
  • davebullockmbe
    davebullockmbe over 1 year ago in reply to anniel747 +2 verified
    Interesting thanks :-)
  • misaz
    0 misaz over 1 year ago

    I do not know standards, but according to https://kiloohm.info/3-digit-capacitor/478 numbers 8 and 9 and dedicated to special cases:

    XY9 is X.Y pF

    XY8 is 0.XY pF

    I have Kemet capactor kit and it match this coding scheme.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 1 year ago in reply to misaz

    The OP's part is a Kemet part, so it's no surprise if the capacitor kit matches the same scheme as the OP's part.

    One would have to pay for the latest standards, but there's a PDF 1971 version of EIA RS-198 which indicates a three-digit code. None of the low-value capacitors that I have observe that to the letter.

    According to the Yageo/Kemet chart that was pasted earlier, the zero is not stated to be optional and yet countless ceramic disc capacitors display fewer digits for the low values.

    I've checked a Vishay 22pF leaded MLCC I have here, it does not append a zero for the third digit either.

    I also checked some Wima polypropylene capacitors here, same story.

    Also, a TDK spec also mentions using an R for the decimal place for leaded MLCC (as does Murata for leaded MLCC, as mentioned further up).

    I think it's safe to say the precise coding method may well vary depending on manufacturer or where their product line or factory originated from, or simply age of the component, if the specs changed, or if they later decided to adhere to a particular standard or revision.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<