Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum MikroBus GPIO
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 334 subscribers
  • Views 1234 views
  • Users 0 members are here
  • lcd
  • gpio
  • mikrobus
  • ZUBoard
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

MikroBus GPIO

MATRIX7878
MATRIX7878 over 1 year ago

Hello,

     I am using a ZuBoard 1CG and am trying to use the MikroBus as GPIO pins so I can program a parallel LCD screen.  I am getting strange signals coming out of the pins.  Even just alternating GPIO signals creates strange results.  There are large multi-second gaps for some lines, some have random switches and some keep running forever despite a stop condition.  From the schematic, the only IC between the SoC and MikroBus connector is a 1.8 V to 3.3 V converter.  Why would I have strange behavior?

Thank you

  • Sign in to reply
  • Cancel

Top Replies

  • electronicbiker
    electronicbiker over 1 year ago +1
    It sounds like an open connection somewhere, possibly an 'enable/disable' pin or the like. Or perhaps if your cables are too long and/or are not screened and some interference is getting onto them from…
  • javagoza
    javagoza over 1 year ago +1
    Have you checked your design and outputs using the integrated logic analyzer (ILA)? It's easy to add an ILA to your design, and you'll know for sure whether it's a digital design error or a board error…
Parents
  • MATRIX7878
    0 MATRIX7878 over 1 year ago

    There is no enable/disable pin and the cables connected to MikroBus and the LCD are no longer than three inches.

    This is the converter:

    image

    I cannot short any of the connections for the MikroBus as they go straight from the SoC, to the voltage converter, to the MikroBus.  I have measured the voltage going into the converter and it measures 1.8V.  The VDD_CLICK voltage is 2.5-3.0V.  None of the pins are generators, they are all I/O.

    Is this the joint you are referring to?

    image

    If so, they stopped soldering on that part it seems.  Other than that, there are no SMD midair pins.  The board I have is less than two months old.  I would highly doubt that they would still have that same mistake now a days.

    I do appreciate your efforts, thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • MATRIX7878
    0 MATRIX7878 over 1 year ago

    There is no enable/disable pin and the cables connected to MikroBus and the LCD are no longer than three inches.

    This is the converter:

    image

    I cannot short any of the connections for the MikroBus as they go straight from the SoC, to the voltage converter, to the MikroBus.  I have measured the voltage going into the converter and it measures 1.8V.  The VDD_CLICK voltage is 2.5-3.0V.  None of the pins are generators, they are all I/O.

    Is this the joint you are referring to?

    image

    If so, they stopped soldering on that part it seems.  Other than that, there are no SMD midair pins.  The board I have is less than two months old.  I would highly doubt that they would still have that same mistake now a days.

    I do appreciate your efforts, thank you.