Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Intel i960 JD3V66 (NG80960JD3V66) Embedded System Design Issues—Clock and Interrupt Configuration?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 336 subscribers
  • Views 1025 views
  • Users 0 members are here
  • JD3V66
  • NG80960JD3V66
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Intel i960 JD3V66 (NG80960JD3V66) Embedded System Design Issues—Clock and Interrupt Configuration?

nenefly
nenefly over 1 year ago

Hi everyone,

I’m developing an industrial control board based on the Intel i960 NG80960JD3V66 (32-bit RISC, 66MHz, 132-QFP package). During hardware debugging, I’ve run into a few issues and would appreciate advice from anyone with experience:

  1. Clock Configuration
    The datasheet mentions an external clock source but doesn’t clarify whether PLL multiplication is supported. My current design uses a 33MHz crystal, hoping to generate 66MHz via internal PLL:

    • Is there a specific register that needs to be configured to enable the PLL?

    • Are there any known clock jitter limits?

  2. Interrupt Controller

    • Is interrupt priority fixed in the i960 JD series (e.g., IRQ0 highest)?

    • In RISC mode, what’s the typical interrupt latency? The datasheet only states “≤10 cycles,” but my tests show ~15 cycles (no cache hits).

  3. Unused Pin Handling

    • The 132-QFP package has several reserved pins (e.g., RSVD1-4), and the datasheet recommends “leave floating.” But in a high-noise environment, should they be pulled up/down?

Additional Info:

  • Toolchain: Green Hills MULTI 4.1.5 (legacy version with i960 support).

  • Hardware: Custom 4-layer PCB, power supply noise <50mVpp.

Attempted Solutions:

  • Directly connected 33MHz crystal to CLKIN—core fails to start.

  • Interrupt latency test code (based on manual examples), results are inconsistent.

Has anyone worked with this legacy MPU? Or know where to find more detailed app notes?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 1 year ago +1
    May I ask why you are developing a new board for an obsolete and very low performance processor ? MK
Parents
  • shabaz
    0 shabaz 10 months ago

    Hi, you mention:

    • Directly connected 33MHz crystal to
    • CLKIN—core fails to start.
    • Interrupt latency test code (based on
    • manual examples), results are inconsistent.

    How can the "Interrupt test code" be run if the core was not running? 

    Also, are you sure you're actually using that part; there are only 9 currently in stock at DigiKey at $35 each, but if you're using an old one from say AliExpress or eBay it could be faulty or fake anyway.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz 10 months ago

    Hi, you mention:

    • Directly connected 33MHz crystal to
    • CLKIN—core fails to start.
    • Interrupt latency test code (based on
    • manual examples), results are inconsistent.

    How can the "Interrupt test code" be run if the core was not running? 

    Also, are you sure you're actually using that part; there are only 9 currently in stock at DigiKey at $35 each, but if you're using an old one from say AliExpress or eBay it could be faulty or fake anyway.