Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Stray readings on my XDM 1041 Multi Meter
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 336 subscribers
  • Views 1511 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Stray readings on my XDM 1041 Multi Meter

FreeBird
FreeBird 11 months ago

I just want to confirm my suspicions.

I recently read an article by Forrest Mims regarding using LED's as light detectors.  I decided to see how my cheap chinese LED's would react so I plugged 2 wires into 2 adjacent rows on one of my bread boards.  Connected my DMM to them.  I then selected 1 of each color LED from my kit which contains 5 different colors (Red, Blue, Yellow, White and Green).  I noticed however, that I was getting stray voltage readings with nothing connected in the bread board.  I decided to record a series of 500 readings to see what the min, max and average of them would be.  This is what I got:

Min -0.0003
Max 0.0001
Average

-0.000025

I suspect, but would like someone smarter than me to confirm, that this is stray EMF in my lab.  I have a window AC unit running, my computer, a florescent light, etc.  Am I correct in my suspicion?  How might I confirm this, other than asking that is?

Thanks 

Charlie

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz 11 months ago in reply to shabaz +4
    Curiosity got the better of me, I decided to get off my backside and retrieve the multimeter. Rubbing a piece of plastic onto t-shirt (I used a ruler) and placing the multimeter negative lead near it,…
  • beacon_dave
    beacon_dave 11 months ago +3
    May also be of interest: Experimenting With Using an LED as a Light Sensor More on Using an LED as a Light Sensor
  • shabaz
    shabaz 11 months ago +2
    Hi, An ideal voltmeter will have infinite impedance, so technically even static charges will cause a non-zero measurement, there's no need for it to be electromagnetic interference. In fact, multimeters…
Parents
  • shabaz
    shabaz 11 months ago

    Hi,

    An ideal voltmeter will have infinite impedance, so technically even static charges will cause a non-zero measurement, there's no need for it to be electromagnetic interference. In fact, multimeters do not make good EMI measurement devices at all.

    It's very normal for most multimeters to display a value when not connected to a circuit, or not shorted. If you short the two test leads, you'll see the measurement become zero (or extremely close to zero).

    To demonstrate that it is static charges, you could try rubbing a balloon with hair, and then hover one lead close to the balloon and gently move it around hovered over the surface, because those static charges will dissipate since the multimeter doesn't quite have infinite resistance. I've not tried this experiment, but I suspect you'll see non-zero measurements. Anyway, do report back the results, it's an interesting question.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz 11 months ago

    Hi,

    An ideal voltmeter will have infinite impedance, so technically even static charges will cause a non-zero measurement, there's no need for it to be electromagnetic interference. In fact, multimeters do not make good EMI measurement devices at all.

    It's very normal for most multimeters to display a value when not connected to a circuit, or not shorted. If you short the two test leads, you'll see the measurement become zero (or extremely close to zero).

    To demonstrate that it is static charges, you could try rubbing a balloon with hair, and then hover one lead close to the balloon and gently move it around hovered over the surface, because those static charges will dissipate since the multimeter doesn't quite have infinite resistance. I've not tried this experiment, but I suspect you'll see non-zero measurements. Anyway, do report back the results, it's an interesting question.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz 11 months ago in reply to shabaz

    Curiosity got the better of me, I decided to get off my backside and retrieve the multimeter. Rubbing a piece of plastic onto t-shirt (I used a ruler) and placing the multimeter negative lead near it, causes a very noticeable positive measurement (lower than a volt though, since the multimeter impedance isn't infinite). Can hold the lead near the plastic, and continually rub the plastic on cloth, and the reading is sustained. The positive lead was going nowhere, it was just left alone nearby.

    • Cancel
    • Vote Up +4 Vote Down