Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Do I need to add more components to make this transformer safer?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 1 answer
  • Subscribers 335 subscribers
  • Views 714 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Do I need to add more components to make this transformer safer?

HKPhysicist
HKPhysicist 5 months ago

Dear all Electrical and Electronic Engineers,

I own an audiophile grade Sony blue disc player.  It accept 115V AC.

Then, I bought this transformer which transforms my wall outlet 230V AC to 115V AC, which is then connected to my Sony Disc Player.

https://hk.element14.com/triad-magnetics/vpt230-110/transformer-toroidal-2-x-115v/dp/1785731

Do you think whether I need to add additional components to make this transformer safer to work?  I have already bought another beautiful aluminium enclosure to contain it.  Grinning

The main point is - it is an audiophile grade system.  Additional components may degrade the final sound quality.

So, there is a dilemma.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett 5 months ago in reply to HKPhysicist +4
    The only way you will hear any difference is (perhaps) if you drop them both on the floor. The transformer you have chosen should be fine if it's power rating is sufficient (25VA sounds very low for…
  • robogary
    robogary 5 months ago +3 suggested
    No dilemma at all. IMHO, if you have an audiophile player, it has no audio power amplifier. As long as your power supply can supply the power peaks of the dynamic range, its OK. That being said, 25 VA…
Parents
  • robogary
    0 robogary 5 months ago

    No dilemma at all. IMHO, if you have an audiophile player, it has no audio power amplifier. As long as your power supply can supply the power peaks of the dynamic range, its OK.

    That being said, 25 VA at 115 VAC is only about 210 mA.

    Transformer spec says 220mA FLA. I dont know what your player power requirements are, but just for giggles pretend the 25 VA is unity PF, i.e. watts. So the transformer rated maybe ok. I have a cheapo blue ray player with HDMI output that uses 10W, 12V at 800 mA. 

    Anyway to get to the real point of your question, transformers, motors, etc are often fused unless they are impedance protected, i.e. their impedance is high enough that a short circuit doesnt overload the wiring. 

    This transformer has 12% voltage regulation from no load to full load, so without doing calcs, Id swagger short circuit current is enough that Id want to fuse the primary.  600mA to 1A slo blo would do the job. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • geralds
    0 geralds 5 months ago in reply to robogary

    ..."Der Transformator-Spezifikation sagt 220 mA FLA. Ich weiß nicht, wie dein Leistungsbedarf für die Spieler ist, aber nur zum Spaß tu so, als wären die 25 VA Unity PF, also Watt. Der Transformator ist also vielleicht in Ordnung. Ich habe einen günstigen Blue-Ray-Player mit HDMI-Ausgang, der 10W und 12V bei 800 mA verbraucht."

    Please don't merge two values: 10W / 12V/800mA DC is not the same as 115V/220mA AC.

    Relatively, in his calculation with your player - in his player (i don't know??) is built-in a power supply, as well as a controller with buttons, a display, etc.. which need also a bit of "water".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • geralds
    0 geralds 5 months ago in reply to robogary

    ..."Der Transformator-Spezifikation sagt 220 mA FLA. Ich weiß nicht, wie dein Leistungsbedarf für die Spieler ist, aber nur zum Spaß tu so, als wären die 25 VA Unity PF, also Watt. Der Transformator ist also vielleicht in Ordnung. Ich habe einen günstigen Blue-Ray-Player mit HDMI-Ausgang, der 10W und 12V bei 800 mA verbraucht."

    Please don't merge two values: 10W / 12V/800mA DC is not the same as 115V/220mA AC.

    Relatively, in his calculation with your player - in his player (i don't know??) is built-in a power supply, as well as a controller with buttons, a display, etc.. which need also a bit of "water".