Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum 18650 Li ion batteries question
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Locked Locked
  • Replies 11 replies
  • Subscribers 336 subscribers
  • Views 412 views
  • Users 0 members are here
  • 18650_battery
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

18650 Li ion batteries question

dubbie
dubbie over 4 years ago

I have been gifted a (broken) child's electric tricycle toy. The main problem is that the 6V 4Ah lead acid battery is defective - a collapsed cell I assume. I would like to replace this battery with Li-Ion batteries, specifically the 18650 type. I am thinking of using two 18650 to get the 6V needed (it will be a bit more at 7.2V but that will just mean the tricycle goes faster - Yeah!). However, I am finding it difficult to find suitable 18650 batteries and associated charger. It is not clear what the capacity of these 18650 batteries is. Do they vary? What is the maximum capacity? I have seen 3300 mAh mentioned but I'm having trouble identifying these batteries. I could create a parallel series arrangement of batteries to get higher currents but then I do not seem to be able to find a charger. I'd like to have separate 18650 batteries so I can use them in other things such as mobile robots.

 

I thought of using a 7.2V battery pack as used in cordless drills, but I cannot find any at 7.2V (or is it 7.4V - but I cannot find any of them either), plus I'm reluctant to spend a fair bit of money without knowing if it would be suitable or not.

 

Any advice or sources of information would be welcome.

 

Dubbie

  • Cancel
Parents
  • rsjawale24
    0 rsjawale24 over 4 years ago

    Hi! The battery capacity varies as per manufacturer. Even for the 18650 type, they are available in different capacity.

    I recommend to buy from a vendor that gives a datasheet along with the battery.

    Also, since this is a Li-ion battery, you'll need a specific charger for this. I think a generic Li-ion charger can work fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • rsjawale24
    0 rsjawale24 over 4 years ago in reply to rsjawale24

    MiniZeroCam This blog by maxpowerr uses a TP4056 based Li battery charger. It's a generic one and inexpensive.

    This vendor (https://www.addicore.com/TP4056-Charger-and-Protection-Module-p/ad310.htm ) is selling one for about USD 1.2 along with the datasheet. 

    Surprisingly, it's available for much lower price (INR 24 ~ USD 0.32) in some online Indian stores

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
Reply
  • rsjawale24
    0 rsjawale24 over 4 years ago in reply to rsjawale24

    MiniZeroCam This blog by maxpowerr uses a TP4056 based Li battery charger. It's a generic one and inexpensive.

    This vendor (https://www.addicore.com/TP4056-Charger-and-Protection-Module-p/ad310.htm ) is selling one for about USD 1.2 along with the datasheet. 

    Surprisingly, it's available for much lower price (INR 24 ~ USD 0.32) in some online Indian stores