Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum How to use a Monitor with Display Port on Raspberry Pi 5
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • +1 person also asked this people also asked this
  • Replies 3 replies
  • Subscribers 337 subscribers
  • Views 688 views
  • Users 0 members are here
  • connector
  • hdmi
  • cable
  • raspberrypi
  • Other
  • switch
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

How to use a Monitor with Display Port on Raspberry Pi 5

perryaire
perryaire 3 months ago

For about 20 years I used a KVM switch that switched monitors that had DVI connectors, I as able to connect my RaspberryPi 5 through this switch using a cable that had micro HDMI on one end a DVI on the other. The DVI KVM Switch failed and is not replaceable. I have replaced it with a KVM switch that switches monitors with Display Port. I managed to connect my Windows and Mac computers using this switch (requires complete recabling) but I am having trouble with the Raspberry Pi. I have a micro Hdmi to hdmi adapter to which I connect an Hdmi to Display port cable. These two cables together are connected to the KVM pitch input. Kvm Switch output is connected to monitors (display port to display port). The Pi boots but the desktop does not display on the monitor.

I know the Pi is still working. I tested using a TV that has Hdmi inputs and the Pi ends up wonting through the switch for Keyboard and Mouse and the TV for monitor. The Pi does not display on the switched monitor. I would like to be able to use the pi through the switch. Anybody have any thoughts on what is preventing the signal from reaching the monitor?

Thanks in advance for any suggestions.

Perry Sugerman

Downers Grove, IL

  • Sign in to reply
  • Cancel

Top Replies

  • Qbit
    Qbit 3 months ago +3 verified
    Hi Perry, The culprit here is likely the HDMI-to-DisplayPort cable. Standard cables you find online are unidirectional and only work to connect a DisplayPort computer to an HDMI monitor—not the other…
  • kmikemoo
    0 kmikemoo 3 months ago

    perryaire I do not have a Pi5.  A few years back, I did use a Pi with a HDMI to VGA adapter.  The display would not show during boot, but would come to life once the system was up and running.  I just assumed that the adapter needed time to figure things out.  From checking the forums, this may not help with your Pi5.  You may need to set the video output up separately.
    https://forums.raspberrypi.com/viewtopic.php?t=367012

    This may also give you an answer as to why your current setup is not working.  Good luck!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Qbit
    +1 Qbit 3 months ago

    Hi Perry,

    The culprit here is likely the HDMI-to-DisplayPort cable. Standard cables you find online are unidirectional and only work to connect a DisplayPort computer to an HDMI monitor—not the other way around.

    Because the Pi outputs HDMI and your KVM expects DisplayPort, you will need to look for an Active HDMI to Display Port ,these usually have a built-in USB cable for external power to drive the chip.

    Also, make sure you are plugged into the HDMI 0 port on the Pi 5 (the micro-HDMI port nearest to the USB-C power jack), as it handles the primary display handshake much better when running through switches!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • colporteur
    0 colporteur 3 months ago

    It works sometimes!

    Last year I worked with HDMI and Display port switches to stream video using a Raspberry Pi 5. What I discovered is that newer technology i.e.higher HDMI and DP standard don't work on older stuff like Pi's. 

    The switches themselves created issues. One manufacture would work and the other wouldn't. DP into a switch would support HDMI out but on another vendor it would not. The different DP standards themselves create issues.

    I found devices that had little smarts had the least problems. Any device that had features the Pi never worked.

    At the end of the week, I did manage to take DP video->DP switch->HDMI switch->Pi--> video streaming device but it was not sustainable. Oh did I mention the monitors themselves add a variables to the mix. HDMI & DP ports on monitors don't behave the way you think.

    I feel I have experienced the problems you are having. Unfortunately I don't have a "here use this" solution. It is device, standards and technology related. Amazon has great pictures of streaming devices but getting them to work outside the normal Windows world was a bust.