Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Make: Electronics Second Edition.   Experiment 11 NO SOUND!
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 305 subscribers
  • Views 1210 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Make: Electronics Second Edition.   Experiment 11 NO SOUND!

computerhabit
computerhabit over 8 years ago

The Experiment is called "Light and Sound".

 

It has you walk through setting up some Transistors to make an LED blink.  Then you swap out some resistors and add a capacitor to make the LED fade out.

 

Then it says:

 

Remove the LED, the 470-ohm resistors, and the 220µF capacitor, and substitute a little loudspeaker, a 100µF coupling capacitor, and a 1K resistor.

 

First, there is no explanation of what a 'coupling' capacitor is compared to a regular capacitor.  I bought a kit so I'm not sure if I'm using the wrong capacitor or not.  There all little cans except for these tiny orange and a blue one which are kind of square and the regular round ceramic capacitors.

 

I get absolutely no sound.  Just a click and a pop sound and only when add power quickly.

 

I thought maybe if I went further with the instructions I'd get something so I completed the build further down where you basically repeat the build above with additional resistors and adding the speaker.  Still no sound!

 

No clue what I'm doing wrong.  I verified the speaker works by testing it with my set of "Snap Circuits".

  • Sign in to reply
  • Cancel

Top Replies

  • computerhabit
    computerhabit over 8 years ago in reply to beacon_dave +3
    Thank you. This reminded me that in the book they mention that replacing the 3.3 uf capacitors with .01 capacitors to move into a frequency you can hear.
  • computerhabit
    computerhabit over 8 years ago +2
    Thank you to all that responded. I feel kind of silly. As I was banging my head against the desk the positive wire of the speaker fell off! The soldering job on the speaker was bad and failed, I guess…
  • computerhabit
    computerhabit over 8 years ago in reply to COMPACT +1
    Thank you for the part about doing away with the coupling capacitor. That is how I was able to get my first sounds.
Parents
  • beacon_dave
    beacon_dave over 8 years ago

    The bit of text in the book you are looking for is this:

     

    "The capacitor blocks the DC component of the signal, while allowing the alternating current through."

     

    It is describing the function/purpose of the capacitor as opposed to its design type.

     

    The breadboard diagram (Figure 2-120) shows an aluminium electrolytic capacitor being used, which matches the preamble text about components.

     

    What is a Coupling Capacitor?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • computerhabit
    computerhabit over 8 years ago in reply to beacon_dave

    Thank you for responding.  I still don't see where my issue is.  Can you at least tell me that you completed this experiment and you got sound?

     

    Honestly I'm thinking there is something missing from the book.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago in reply to computerhabit

    I've not even read the book - but looking at the page you refer to, it looks like an astable multivibrator circuit initially driving a LED and then driving a small loudspeaker.

     

    First question would be if the multivibrator stage is oscillating.

    Second question would be if the LED is flashing.

    Third question would be if the oscillation frequency is within the audible range of human hearing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • beacon_dave
    beacon_dave over 8 years ago in reply to computerhabit

    I've not even read the book - but looking at the page you refer to, it looks like an astable multivibrator circuit initially driving a LED and then driving a small loudspeaker.

     

    First question would be if the multivibrator stage is oscillating.

    Second question would be if the LED is flashing.

    Third question would be if the oscillation frequency is within the audible range of human hearing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • computerhabit
    computerhabit over 8 years ago in reply to beacon_dave

    Thank you.  This reminded me that in the book they mention that replacing the 3.3 uf capacitors with .01 capacitors to move into a frequency you can hear.

    • Cancel
    • Vote Up +3 Vote Down