Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum How can I simulate a button press
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 327 subscribers
  • Views 3841 views
  • Users 0 members are here
  • board
  • wire to wire
  • button
  • press
  • simple
  • long click
  • short
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

How can I simulate a button press

dzavoo
dzavoo over 8 years ago

Hey!

I am new to this field and I may not understand some terminology correctly, anyways,

 

Currently I am working on a project that releases smoke when the on/off button is pressed, I need to simplify the mechanism

and I want it to immediately start working when I plug it in to power source (without physically pressing the button).

 

I tried removing button entirely from the mechanism and I connected the "in" and "out" wires directly to each other

(without connecting them with a button) but it registered as a long button press, I need it to register something like a short impulse, like the physical button does.

 

How, and with what, should i connect the "in" and "out" wires together so it will trigger and simulate a short button press?

I dont have any access to board's software so i have to do something with the hardware or i can add another board to the system.

 

Thank you very much!!

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +3
    You should be able to create a power-on pulse with a capacitor and maybe a resistor. If the button shorts out a signal to ground, then just a capacitor where the button was will "keep the button pushed…
  • anansi22
    anansi22 over 8 years ago +2
    Hi David, Couple of this come to mind. 1. You could try wiring in a relay instead of the switch. If you want to simulate a button press you could McGuyver a setup with a capacitor and relay. Once the relay…
Parents
  • dougw
    dougw over 8 years ago

    You should be able to create a power-on pulse with a capacitor and maybe a resistor.

    If the button shorts out a signal to ground, then just a capacitor where the button was will "keep the button pushed" for a short time. A large resistor across the capacitor will ensure it gets reset for the next power on sequence.

    If the button supplies power when pushed, again putting a capacitor where the button was will cause a "button push" on power-up. In this scenario a resistor may be needed from the output to ground to make sure the capacitor signal goes away in a reasonable time.

    If the capacitor is large, you might want a diode to ensure the signal doesn't go negative.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 8 years ago

    You should be able to create a power-on pulse with a capacitor and maybe a resistor.

    If the button shorts out a signal to ground, then just a capacitor where the button was will "keep the button pushed" for a short time. A large resistor across the capacitor will ensure it gets reset for the next power on sequence.

    If the button supplies power when pushed, again putting a capacitor where the button was will cause a "button push" on power-up. In this scenario a resistor may be needed from the output to ground to make sure the capacitor signal goes away in a reasonable time.

    If the capacitor is large, you might want a diode to ensure the signal doesn't go negative.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dzavoo
    dzavoo over 8 years ago in reply to dougw

    Thank you!

    but what type of resistor and capacitor would you recommend and in what size?

     

    The button I need to replace is similiar to this one goo.gl/EVZgWd

    and my entire machine uses only 1W of power

    • Cancel
    • Vote Up 0 Vote Down