Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Voltage reduction
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 307 subscribers
  • Views 3061 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Voltage reduction

Andy Betts
Andy Betts over 7 years ago

i build guitar effects pedals for a hobbie, and I have a modification I'd like to carry out and i'm hoping some of you may be able to guide me with a solution.

 

Ok... Here's my plan. I have 2 effects pedals... An electric mistress which runs on 18v (it actually has a voltage regulator inside it with reduces the voltage to around 13v but it does run on 2 9v batteries), the second pedal is a boost pedal which runs a single 9v battery which i currently run after the electric mistress to boost the output. The problem with the electric mistress is when you engage the effect the output volume drops by around 10 to 15%, so the boost pedal compensates for that drop.

 

What i want to do is build the boost circuit into the electric mistress enclosure.. so the guitar will go into the electric mistress travel through the mistress circuit to the output of the circuit then into the boost circuit, then to the output jack socket. Simple, but i have a dilema inso far as they each run on different voltages, so how can i regulate the 18v DC down to 9vdc for the boost part of the circuit? If they both ran on the same voltage it'd be easy.... but i'm a little lost with this.

 

I've been told to use a resistor but I've also been told that's not the right way to do it.... Any ideas?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 7 years ago in reply to jc2048 +9
    Hi Jon, I have run a three simple tests and here are the results. I have Breadboarded an LM7809 on the left of the breadboard and a Recom R78C9.0-1.0 on the right side. Both have been provided with input…
  • genebren
    genebren over 7 years ago in reply to genebren +7
    Andy, I found the schematic that you had posted awhile ago (TL061 op-amp), and it looks like the circuit will operate at 18V. The only thing that you might need to check are the voltage ratings on you…
  • three-phase
    three-phase over 7 years ago +6
    I believe a simple 9V DC regulator will achieve what you need. You will be able to feed the 18V into this and it will produce the 9V output to run the boost pedal. L7809 9V/1.5A regulator The device above…
Parents
  • geralds
    geralds over 7 years ago

    It seems that the electrical mistress works with a single voltage of about 13V. ? -13V a little outside the norms, near 12V or 15V ,,, hm ....
    Well, then you can do a split voltage - two 9V batteries in series, the middle contact supplies the booster.
    How much voltage does the booster withstand, or what are the tolerances of the supply voltage? Up to 13V or 14V would be the optimum.
    Important - how much current do these modules need during peak loads?
    Well, the lower battery is slightly more loaded than the upper one.
    That's when the batteries are used as splitter voltage.

    Or supply both modules of the 18V, each with their own voltage regulators (DC-DC PS with two outputs).
    But then you have for the 9V a little more heat in the controller because of power loss.
    For this, the batteries are not charged differently, which is better for the batteries.
    Two regulators in serial is the same as two batteries in serial circuit. Here the 13V regulator will be more loaded, similar as the lower battery.

     

    In both options you have almost the same mechanical effort, either more batteries, or a regulator.

    But with a one-voltage battery (15,,18,,,3000000) you are a bit more flexible with the following circuits.

    With a dual-voltage power supply you have twice as much effort to solve.

     

     

    Edit:
    LDO regulators would be a good alternative to the switching regulators.
    So if you choose these with very small drop-voltage, then they are really alternative and also very small in space.

     

    Best Regards

    Gerald

    ---

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • geralds
    geralds over 7 years ago

    It seems that the electrical mistress works with a single voltage of about 13V. ? -13V a little outside the norms, near 12V or 15V ,,, hm ....
    Well, then you can do a split voltage - two 9V batteries in series, the middle contact supplies the booster.
    How much voltage does the booster withstand, or what are the tolerances of the supply voltage? Up to 13V or 14V would be the optimum.
    Important - how much current do these modules need during peak loads?
    Well, the lower battery is slightly more loaded than the upper one.
    That's when the batteries are used as splitter voltage.

    Or supply both modules of the 18V, each with their own voltage regulators (DC-DC PS with two outputs).
    But then you have for the 9V a little more heat in the controller because of power loss.
    For this, the batteries are not charged differently, which is better for the batteries.
    Two regulators in serial is the same as two batteries in serial circuit. Here the 13V regulator will be more loaded, similar as the lower battery.

     

    In both options you have almost the same mechanical effort, either more batteries, or a regulator.

    But with a one-voltage battery (15,,18,,,3000000) you are a bit more flexible with the following circuits.

    With a dual-voltage power supply you have twice as much effort to solve.

     

     

    Edit:
    LDO regulators would be a good alternative to the switching regulators.
    So if you choose these with very small drop-voltage, then they are really alternative and also very small in space.

     

    Best Regards

    Gerald

    ---

    • Cancel
    • Vote Up +3 Vote Down