Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Voltage reduction
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 307 subscribers
  • Views 3074 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Voltage reduction

Andy Betts
Andy Betts over 7 years ago

i build guitar effects pedals for a hobbie, and I have a modification I'd like to carry out and i'm hoping some of you may be able to guide me with a solution.

 

Ok... Here's my plan. I have 2 effects pedals... An electric mistress which runs on 18v (it actually has a voltage regulator inside it with reduces the voltage to around 13v but it does run on 2 9v batteries), the second pedal is a boost pedal which runs a single 9v battery which i currently run after the electric mistress to boost the output. The problem with the electric mistress is when you engage the effect the output volume drops by around 10 to 15%, so the boost pedal compensates for that drop.

 

What i want to do is build the boost circuit into the electric mistress enclosure.. so the guitar will go into the electric mistress travel through the mistress circuit to the output of the circuit then into the boost circuit, then to the output jack socket. Simple, but i have a dilema inso far as they each run on different voltages, so how can i regulate the 18v DC down to 9vdc for the boost part of the circuit? If they both ran on the same voltage it'd be easy.... but i'm a little lost with this.

 

I've been told to use a resistor but I've also been told that's not the right way to do it.... Any ideas?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 7 years ago in reply to jc2048 +9
    Hi Jon, I have run a three simple tests and here are the results. I have Breadboarded an LM7809 on the left of the breadboard and a Recom R78C9.0-1.0 on the right side. Both have been provided with input…
  • genebren
    genebren over 7 years ago in reply to genebren +7
    Andy, I found the schematic that you had posted awhile ago (TL061 op-amp), and it looks like the circuit will operate at 18V. The only thing that you might need to check are the voltage ratings on you…
  • three-phase
    three-phase over 7 years ago +6
    I believe a simple 9V DC regulator will achieve what you need. You will be able to feed the 18V into this and it will produce the 9V output to run the boost pedal. L7809 9V/1.5A regulator The device above…
Parents
  • genebren
    genebren over 7 years ago

    Andy,

     

    I would not know without looking at the schematic, but sometimes it is possible to run circuits from higher voltages (i.e. it might be possible to run both circuits from the same source).  You would have to determine if all of the circuits on the low voltage board could be driven from the higher voltage (i.e. transistors, etc.). Also you would need to look at any biasing circuits to see if they would function at the higher voltage.

     

    Good luck,

    Gene

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 7 years ago in reply to genebren

    Andy,

     

    I found the schematic that you had posted awhile ago (TL061 op-amp), and it looks like the circuit will operate at 18V.  The only thing that you might need to check are the voltage ratings on you capacitors.

     

    Gene

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • Andy Betts
    Andy Betts over 7 years ago in reply to genebren

    All my caps are rated at 50v minimum. Some as high as 100v, it all depends on the physical size of the capacitor. Sometimes i'm being led by size and what will look good on the board, in a lot of cases on vintage pedals they use 1/2w resistors so bigger than normal 1/4w, and also they tend to use 100v caps, therefore they are normally bigger. On the booster that I built i used small 1/4w resistors, and 50v caps

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Andy Betts
    Andy Betts over 7 years ago in reply to genebren

    All my caps are rated at 50v minimum. Some as high as 100v, it all depends on the physical size of the capacitor. Sometimes i'm being led by size and what will look good on the board, in a lot of cases on vintage pedals they use 1/2w resistors so bigger than normal 1/4w, and also they tend to use 100v caps, therefore they are normally bigger. On the booster that I built i used small 1/4w resistors, and 50v caps