Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Voltage reduction
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 307 subscribers
  • Views 3051 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Voltage reduction

Andy Betts
Andy Betts over 7 years ago

i build guitar effects pedals for a hobbie, and I have a modification I'd like to carry out and i'm hoping some of you may be able to guide me with a solution.

 

Ok... Here's my plan. I have 2 effects pedals... An electric mistress which runs on 18v (it actually has a voltage regulator inside it with reduces the voltage to around 13v but it does run on 2 9v batteries), the second pedal is a boost pedal which runs a single 9v battery which i currently run after the electric mistress to boost the output. The problem with the electric mistress is when you engage the effect the output volume drops by around 10 to 15%, so the boost pedal compensates for that drop.

 

What i want to do is build the boost circuit into the electric mistress enclosure.. so the guitar will go into the electric mistress travel through the mistress circuit to the output of the circuit then into the boost circuit, then to the output jack socket. Simple, but i have a dilema inso far as they each run on different voltages, so how can i regulate the 18v DC down to 9vdc for the boost part of the circuit? If they both ran on the same voltage it'd be easy.... but i'm a little lost with this.

 

I've been told to use a resistor but I've also been told that's not the right way to do it.... Any ideas?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 7 years ago in reply to jc2048 +9
    Hi Jon, I have run a three simple tests and here are the results. I have Breadboarded an LM7809 on the left of the breadboard and a Recom R78C9.0-1.0 on the right side. Both have been provided with input…
  • genebren
    genebren over 7 years ago in reply to genebren +7
    Andy, I found the schematic that you had posted awhile ago (TL061 op-amp), and it looks like the circuit will operate at 18V. The only thing that you might need to check are the voltage ratings on you…
  • three-phase
    three-phase over 7 years ago +6
    I believe a simple 9V DC regulator will achieve what you need. You will be able to feed the 18V into this and it will produce the 9V output to run the boost pedal. L7809 9V/1.5A regulator The device above…
Parents
  • jw0752
    jw0752 over 7 years ago

    Hi Andy,

     

    I see two possibilities. #1 you said that the unit runs on (2) 9 volt batteries in series to make 18 volts. If you tap into the connection between the two batteries you will have the required 9 volts. One battery will be running both devices so it would likely fail sooner. #2. If you are going to use a voltage regulator I would recommend that you use the DC to DC converter type as these are more efficient than the linear 7809. Check out the following link

     

    https://www.newark.com/recom-power/r-78e9-0-0-5/dc-dc-converter-9v-0-5a/dp/84Y3692?st=9v%20dc%20power%20supply

     

    With a battery powered device it is a good idea to conserve as much energy as possible. If you used the 18 volt source and had one 12 volt converter and one 9 volt converter both of your batteries would see the same load.

     

    John

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • afmishaq
    afmishaq over 7 years ago in reply to jw0752

    Using a dc-to-dc converter should be the preferred option as it is more efficient. Dropping 18 V to 9 V using a linear regulator means loosing half the power to the heat sink.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 7 years ago in reply to afmishaq

    Have a look at the efficiency of this cheap switching circuit at 10mA. It probably isn't much better than using a linear regulator.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds over 7 years ago in reply to jc2048

    Yes fine alternatives are LDOs.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to jc2048

    Hi Jon,

    I will investigate and compare efficiencies this evening.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to jc2048

    Hi Jon,

    I have run a three simple tests and here are the results.

    I have Breadboarded an LM7809 on the left of the breadboard and a Recom R78C9.0-1.0 on the right side. Both have been provided with input and output capacitors as specified in their data sheets. The power source for this experiment is a series bank of (3) 6.3 volt lead acid gel cells for a total of 18.9 volts. Hopefully this will eliminate power supply fluctuations as a variable.  All meters and loads have been set up left to right to correspond to the relative positions of the DUTs. The Radio Shack and Fluke are set up to read mA with the RS displaying input current for the LM7809 and the Fluke displaying current for the R78C9.0. I was very happy to have a good use for my two new low current loads with the left unit displaying the load on the 7809 and the right unit displaying the load on the R78C9.0. The oscilloscope has the yellow channel 1 on the output of the 7809 and the blue channel is on the output of the R78C9.0. Both oscilloscope channels are set to 20 mV vertical resolution and AC input with the voltage displayed for volts P-P. Here is a picture of the experimental layout.:

     

    image

     

    If you click on the picture you can expand it enough to see most of the details except the scope. I ran three tests, one at 5 mA, another at 10 mA load and finally one at a 20 mA load. Here are the results:

     

    5 mA Load Test

                           7805                            R78C9.0

    V Input            18.8 V                           18.8 V

    I Input               8.7 mA                        3.83 mA

    V Output          8.9 V                            9.1 V

    I Output            5.0 mA                         5.0 mA

    Efficiency         27%                              63%

     

    10 mA Load Test

     

    V Input           18.9 V                          18.9 V

    I Input             13.7 mA                         6.31 mA

    V Output           8.9 V                           9.1 V

    I Output           10 mA                          10 mA

    Efficiency         34%                             76%

     

    20 mA Load Test

     

    V Input             18.8 V                         18.8 V

    I Input              24.2 mA                       11.59 mA

    V Output            8.9 V                            9.1 V

    I Output           20 mA                           20 mA

    Efficiency         39%                              83.5%

     

    Now for the rest of the story. As Jon pointed out the cost for this efficiency is some noise from the R78C9.0 converter. Here is a picture of the oscilloscope:

     

    image

    The LM7809 has noise with spikes of about 6 mV PP and the R78C9.0 has spikes of about 22 mV PP. I tried to get a frequency read on the R78 noise and the best I could see was a range of 50 kHz to 100 kHz as the reading jumped around. It is noted that this is well about audio frequencies and may not affect audio performance.

     

    It seems to me that the difference in efficiencies may double the life of the battery.

     

    I will leave the test set up for an hour or so in case anyone want me to run any further experiments.

     

    John

    • Cancel
    • Vote Up +9 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds over 7 years ago in reply to jw0752

    Thanks,

    This confirms my explanation in the posting to Jon Clift.
    Whereby, the LM7809 is rather a not so good regulator, as it is in the meantime on the market.

    In addition, the own noise of the oscilloscope is added.

    (In your table you wrote 7905 instead of 7809)

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 7 years ago in reply to jw0752

    Wrong again! I'm not having a good week, am I?

     

    The Recom device is certainly better than I expected. How does it do over the useable battery voltage range 18V down to (maybe) 14V?

     

    Bit unfair to me to use a 7809 though - if you'd used a low-power regulator the efficiency figures would have been higher.

     

    Are you using the probes x10? If you switch to x1 you'll get a better view of the noise (your lowest scope range should go down a decade). It's probably a good idea to read each separately as there will be some contamination between the probes.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jc2048
    jc2048 over 7 years ago in reply to jw0752

    Wrong again! I'm not having a good week, am I?

     

    The Recom device is certainly better than I expected. How does it do over the useable battery voltage range 18V down to (maybe) 14V?

     

    Bit unfair to me to use a 7809 though - if you'd used a low-power regulator the efficiency figures would have been higher.

     

    Are you using the probes x10? If you switch to x1 you'll get a better view of the noise (your lowest scope range should go down a decade). It's probably a good idea to read each separately as there will be some contamination between the probes.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Children
  • geralds
    geralds over 7 years ago in reply to jc2048

    Contamination comes also from the main powered components.

    It would better to make all noise tests with battery powering.

     

    The Recom devices have a wide input voltage rail, -> Vin = Vout +3V up to 42V.

    https://www.digikey.at/product-detail/de/recom-power/R-78C9.0-1.0/945-1396-5-ND/2652149

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to jc2048

    Hi jon,

    I suspect that even when you are wrong there is a lot of truth to what you are saying. Thanks for the tip on the X10 probe setting. this should have been obvious to me but sometimes I think linearly when I should be a switcher. I will remember the trick to get another decade.

    John

    • Cancel
    • Vote Up +4 Vote Down