Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Voltage reduction
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 307 subscribers
  • Views 3048 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Voltage reduction

Andy Betts
Andy Betts over 7 years ago

i build guitar effects pedals for a hobbie, and I have a modification I'd like to carry out and i'm hoping some of you may be able to guide me with a solution.

 

Ok... Here's my plan. I have 2 effects pedals... An electric mistress which runs on 18v (it actually has a voltage regulator inside it with reduces the voltage to around 13v but it does run on 2 9v batteries), the second pedal is a boost pedal which runs a single 9v battery which i currently run after the electric mistress to boost the output. The problem with the electric mistress is when you engage the effect the output volume drops by around 10 to 15%, so the boost pedal compensates for that drop.

 

What i want to do is build the boost circuit into the electric mistress enclosure.. so the guitar will go into the electric mistress travel through the mistress circuit to the output of the circuit then into the boost circuit, then to the output jack socket. Simple, but i have a dilema inso far as they each run on different voltages, so how can i regulate the 18v DC down to 9vdc for the boost part of the circuit? If they both ran on the same voltage it'd be easy.... but i'm a little lost with this.

 

I've been told to use a resistor but I've also been told that's not the right way to do it.... Any ideas?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 7 years ago in reply to jc2048 +9
    Hi Jon, I have run a three simple tests and here are the results. I have Breadboarded an LM7809 on the left of the breadboard and a Recom R78C9.0-1.0 on the right side. Both have been provided with input…
  • genebren
    genebren over 7 years ago in reply to genebren +7
    Andy, I found the schematic that you had posted awhile ago (TL061 op-amp), and it looks like the circuit will operate at 18V. The only thing that you might need to check are the voltage ratings on you…
  • three-phase
    three-phase over 7 years ago +6
    I believe a simple 9V DC regulator will achieve what you need. You will be able to feed the 18V into this and it will produce the 9V output to run the boost pedal. L7809 9V/1.5A regulator The device above…
Parents
  • jw0752
    jw0752 over 7 years ago

    Hi Andy,

     

    I see two possibilities. #1 you said that the unit runs on (2) 9 volt batteries in series to make 18 volts. If you tap into the connection between the two batteries you will have the required 9 volts. One battery will be running both devices so it would likely fail sooner. #2. If you are going to use a voltage regulator I would recommend that you use the DC to DC converter type as these are more efficient than the linear 7809. Check out the following link

     

    https://www.newark.com/recom-power/r-78e9-0-0-5/dc-dc-converter-9v-0-5a/dp/84Y3692?st=9v%20dc%20power%20supply

     

    With a battery powered device it is a good idea to conserve as much energy as possible. If you used the 18 volt source and had one 12 volt converter and one 9 volt converter both of your batteries would see the same load.

     

    John

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 7 years ago in reply to jw0752

    This is audio equipment. Batteries are nice and quiet. Why spoil things by putting a switcher in the same box?

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds over 7 years ago in reply to jc2048

    Well I also thought about.

    But high frequency switcher does not interference to the signal.

    Please look into a modern microphone also in there are switcher supplies build in.

    E.g. AKG microphones have booster with three output voltages, boosting from 1.5V battery.

    They are very small as well coming with optimized power consumption.

     

    Best Regards

    Gerald

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 7 years ago in reply to geralds

    OK, I'm wrong then (or perhaps just too old and behind the times). Thanks for putting me right.

     

    But those are very specific to the job and are carefully designed and tested in a way that Andy isn't going to manage. I'd still contend that it's a mistake encouraging him to use a cheap switcher like the Recom devices.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds over 7 years ago in reply to jc2048

    Yes, I agree with you completely.

     

    For him it would be good to use LDOs with very low dropouts.

    And this LDOs would be selected in seeing the electrical current consumption.

    Then may be, then it wouldn't needing a heat sink.

    Regulating via Zener is very inefficient.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rusgray
    rusgray over 7 years ago in reply to geralds

    Your assertion is incorrect. Noise from switching power supplies (even high-frequency ones) can absolutely make its way into an audio signal. There are techniques that can be used to reduce the impact of SMPS noise (e.g. using ferrite beads together with the input/output reservoir capacitors of an LDO (or LDOs) after the SMPS, as in this app note: http://www.analog.com/media/en/technical-documentation/application-notes/an101f.pdf ), but it is still considered bad practice to use only switch-mode devices in audio equipment. I'm currently in the middle of designing an extremely wide-bandwidth, low-noise audio measurement amplifier at work; there will be no switch-mode devices of any kind inside the enclosure.


    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds over 7 years ago in reply to rusgray

    Yes it can. I know this too. I said this as well above.

    http://www.analog.com/media/en/technical-documentation/application-notes/an101f.pdf

     

    Yes of course. High-frequency interference from the switching power supply must be filtered out.

    The point is just how far can you go, how much cost / benefit in the effort you have.

    Highly specialized devices, like your measurement amplifier, are not really comparable to the simple devices, such as these effect devices for loud concert music.

    There is always the question of whether one can hear that, with so much "disturbing" effects that are desired anyway.

     

    In the minds of users is firmly anchored: "cheap, cheaper, cheapest" ... "quality?" hm ,, "what is that?"

     

    Best Regards

    Gerald

    ----

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • geralds
    geralds over 7 years ago in reply to rusgray

    Yes it can. I know this too. I said this as well above.

    http://www.analog.com/media/en/technical-documentation/application-notes/an101f.pdf

     

    Yes of course. High-frequency interference from the switching power supply must be filtered out.

    The point is just how far can you go, how much cost / benefit in the effort you have.

    Highly specialized devices, like your measurement amplifier, are not really comparable to the simple devices, such as these effect devices for loud concert music.

    There is always the question of whether one can hear that, with so much "disturbing" effects that are desired anyway.

     

    In the minds of users is firmly anchored: "cheap, cheaper, cheapest" ... "quality?" hm ,, "what is that?"

     

    Best Regards

    Gerald

    ----

    • Cancel
    • Vote Up +2 Vote Down