Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog Alphabet X’s robots can learn to sort trash
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 3 Dec 2019 7:58 PM Date Created
  • Views 1010 views
  • Likes 6 likes
  • Comments 2 comments
  • environment
  • trash
  • alphabet
  • robotics
  • robot
  • sort
  • machine vision
  • cabeatwell
Related
Recommended

Alphabet X’s robots can learn to sort trash

Catwell
Catwell
3 Dec 2019

Alphabet X’s moonshot division, formerly Google X, has announced a new project, called Everyday Robot, which teaches robots how to perform everyday tasks. The robots can use cameras and advanced machine learning algorithms to see and learn from their surroundings without needing to be coded for every individual movement.

 

image

Alphabet X’s robots can learn to sort trash with little to no mistake. (Image Credit: Everyday Robots)

 

The robots collect and use data from its sensors to understand the surrounding it’s in, which includes what it’s seeing, hearing, and where it is. This allows the robot to safely perform everyday tasks with people in workplace environments.

 

Currently, the team is experimenting with robots that can be useful in workplace environments. Their prototypes are focusing on learning how to sort garbage. It can be quite difficult to teach robots something as simple as grabbing an object like humans can. Alphabet X’s Everyday Robot practices the art of grabbing an object in both the physical and virtual worlds. The laboratory has an area, like a “playpen,” where close to 30 robots are supervised by humans and spend the day sorting garbage into trays for compost, landfill, and recycling.

 

During the night time, Everyday Robot uses virtual robots to practice grabbing objects in simulated buildings. The collected data is then combined with real-word data. This data is then sent to the robots system in an update once every one or two weeks.

 

image

Experimentation goes underway where a robot navigates in an office-like setting. (Image Credit: Everyday Robots)

 

According to Alphabet X’s blog post, robots are starting to be pretty efficient when it comes to sorting trash. Apparently, they make less than 5% of mistakes when sorting trash into containers. In comparison, humans put 20% of trash into the wrong place. Engineers hope the robots will be able to assist in other complex tasks, like helping elderly people in their homes, which could be just a few years away.

 

Even though the robots can perform exceptionally well at their tasks, they’re not ready to replace human workers at garbage recycling plants just yet. During a demonstration, one robot attempted to grab a bowl in front of it but ended up grabbing the air instead, and because it thought it grasped the bowl, it attempted to put it down.

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 6 years ago +1
    There are some neat robots shown here. One day I'm going to get me one of those mobile robot bases with a stick and a head. I expect they can get a bit freaky when they start looking you in the face and…
  • dubbie
    dubbie over 6 years ago

    There are some neat robots shown here. One day I'm going to get me one of those mobile robot bases with a stick and a head. I expect they can get a bit freaky when they start looking you in the face and eyes. It is also pretty difficult to stop the mobile robot part running into people and objects without going really slowly.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • three-phase
    three-phase over 6 years ago

    I wonder what the speed of these robots is compared to humans carrying out the task, are the increased errors from the humans due to the speed that they sort the rubbish at, or lack of concentration / boredom.

     

    Kind regards.