Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog Ant-like Swarm Robot Lifts and Transports Objects Heavier Than Its Weight
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 30 Dec 2025 8:54 PM Date Created
  • Views 1014 views
  • Likes 4 likes
  • Comments 0 comments
  • robotics
  • robot
  • on_campus
  • learning
  • Hanyang University
  • swarm bots
  • university
  • innovation
Related
Recommended

Ant-like Swarm Robot Lifts and Transports Objects Heavier Than Its Weight

Catwell
Catwell
30 Dec 2025

image

The Hanyang researchers microrobot swarm can lift objects and guide insects to food. (Image Credit: Device)

Hanyang University researchers developed an ant-like magnetic microrobot swarm that works together to lift objects heavier than its own weight. According to the team, the robots can adapt to their environment and overcome challenging obstacles. Each tiny bot is fabricated via replica molding and magnetization, ensuring uniform geometry. The team uses a simple process, similar to making ice cubes, to fabricate hundreds of these at the same time.

An individual epoxy-based robot in this swarm is only 600 micrometers tall. It contains ferromagnetic neodymium-iron-boron (NdFeB) microparticles, enabling it to interact with magnetic fields and engage with nearby robots in the swarm. After exposure to magnetic fields from rotating magnets, the tiny bots self-assemble into different configurations.

For example, formations include end-to-end, like a train (head-to-tail), overlapping, like shingles (slipped co-facial), and face-to-face, like fridge magnets. Unlike initial spherical swarm robots, which are limited to point contacts, these ant-like bots form face-to-face connections for improved strength, similar to fully contacting magnets.

image
The swarm can propel an individual robot over an obstacle. (Image Credit: Device)

Connecting eight of these robots enables them to climb walls five times their height. Swarms have propelled individual robots over obstacles, while others have transported objects across water, weighing up to 2,000 times the robots’ body weight. During demonstrations, a 1,000-robot swarm assembled into a buoyant platform on the water’s surface. Afterward, it enveloped a pill 2,000 times heavier than a robot, carrying it across the surface. Such behavior replicates how fire ants form living rafts during floods, demonstrating nature-inspired engineering.

While on land, the swarm ferried loads 350 times heavier than an individual robot’s weight. They also worked together to dismantle blockages in tubes, making them potentially applicable to clearing clogged arteries.

Additionally, the robots safely interact with live organisms. By relying on synchronized movements, the swarm can gently herd ants and pill bugs in certain directions without harming them. They also set up a regular feeding mechanism for superworms by controllably obstructing and permitting food access.

Directing the robot swarm is similar to using magnetic waves to sculpt smoke. The team rotates magnetic fields around the robots to induce spinning in place or circular motions. Adjusting the field strength enables flawless shifts between movement modes.

Have a story tip? Message me here at element14.