Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog Banksy’s “Girl with Red Balloon” Painting Gets Shredded at Auction, but Was it all Just a Stunt?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 9 Oct 2018 7:36 PM Date Created
  • Views 3330 views
  • Likes 8 likes
  • Comments 21 comments
  • prank
  • robotics
  • robot
  • cabeatwell
  • auction
  • art
  • banksy
Related
Recommended

Banksy’s “Girl with Red Balloon” Painting Gets Shredded at Auction, but Was it all Just a Stunt?

Catwell
Catwell
9 Oct 2018

image

The $1.4-million painting was seemingly cut to ribbons using a homemade shredder built into the frame. (Image credit: Sotheby’s)

 

Love him or hate him, Banksy’s art has fetched a high price over the last decade, with artworks such as “Space Girl and Bird” netting $479, 926, “Monkey Detonator” earning $587, 544, and “Keep it Spotless” netting an incredible $1.7-million. The latest auction from Sotheby’s for his “Girl with Red Balloon” brought in $1.4-million, the second highest price paid for one of his works, but that’s not what makes it astounding, as the masterpiece was shredded as soon as the auction gavel hit its base.

 

Hidden inside the frame was a homemade shredder that chewed through the canvas after sounding an alarm. Banksy claimed that if this piece ever went to auction, it would be destroyed, and destroyed it was, but was it all an elaborate trick by the 21st-century artist? The video below provides little insight on how Banksy was able to pull it off, but after looking at whatever tech he used, it seems more suspect that someone in the crowd at the auction was part of the ruse.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The video shows a row of X-ACTO blades positioned close to the base of the frame, along with a brief view of the electronics that make up the internal shredder, which looks like a pair of motors to pull the canvas through the blades and maybe some white battery enclosures at the top. It’s hard to tell what exactly is used when he designed the shredder.

 

Here’s where the speculation comes in- Banksy built that frame for the painting back in 2006, and it has apparently remained closed since that time. Shredders, even the homemade versions, require a steady amount of power to work, so it’s hard to imagine any commercial battery retaining enough power to engage the motors after 12-years. Couple that with a receiver circuit in standby mode waiting to engage the shredder, and the prospect of working drops even lower.

 

Some have suggested that a switch hidden somewhere on the frame was engaged by an accomplice at the show, as there was a report a person was escorted out of the auction after the winning bid was announced. There are too many anomalies floating around the auction, as well as unanswered questions- Why didn’t anybody notice the weight of the frame, or open up the back to see the condition of the canvas or to confirm it was an actual Banksy? After the painting self-shredded, it was immediately taken away. Did those workers know it was safe to move it, what if there were more traps that were yet to be sprung?

 

We may never know what the truth is unless the private owner who purchased the artwork reveals what exactly is inside that frame.

 

I am considering making a shedding picture frame as a project. The utility comes in when you're tired of whatever is in it - shred it. image

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

 

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 7 years ago +4
    Nice puzzle. It's a shame not everything is shown : ) but that keeps the value of the "art" high : ) This is my theory: (orange=motor+belt, blue=rubber rollers, brown=wood sheet fitted during the video…
  • balearicdynamics
    balearicdynamics over 7 years ago +4
    99% it's a stunt but Cabe, I am considering making a shedding picture frame as a project. The utility comes in when you're tired of whatever is in it - shred it. You have suggested me a great project,…
  • mp2100
    mp2100 over 7 years ago +4
    A great stunt. It will make the shredded painting worth even more. It’s not a cross-cut shredder. Straight line cut. I wish I’d been the bidder with $1.4mm. Cha-ching! Sell the shreddedpainting for $14…
Parents
  • shabaz
    shabaz over 7 years ago

    I've been thinking of the legal implications of this.. (I have a qualification in this area but the Banksy scenario is way too complicated for me..). English law has some rules on when a contract is formed, and what happens if the situation changes after offer/acceptance, but there are many significant subtleties for certain situations (e.g. auctions, land sales, etc) which means it really is no longer easy to figure out (and I don't have any online access to legal databases, e.g. case law, which plays a huge role in the UK, nor the time to examine them (it can take many hours or days to even begin to briefly understand a single ruling sometimes).

     

    Contracts in general are weird enough, for example there are some seemingly bizarre situations in UK law like it is possible to accept a contract by fax machine on a Friday night, but actually reject it on a Saturday by posting a letter, and the rejection would in theory take precedence. But the situation would flip and the fax would take precedence had we been talking about Thu and Fri, instead of Fri and Sat.. (all to do with when the acceptance or rejection is deemed to occur, and it is different for faxes and postal letters). Anyway that's a digression..

     

    Anyway, in the Banksy situation if the buyer was unwilling to proceed with the contract, any court action against the auction house and/or seller would only result in financial considerations, since that is the courts usual remedy, for contractual obligations broken. (i.e. they won't ever force Banksy to burn the print and create another copy for the buyer, they'd rather just rule on a sum on money, for breaking the contract, or property damage, etc).

    When the auction occurred, if what was going to occur was not previously brought to the attention of the buyer, then someone (the auction house and/or the seller) simply made a financial risk calculation, about the chances of the buyer rejecting the item after the auction.

     

    I bet it was an easy risk calculation, because who would say no to the chance of now owning a very unique print of the girl+balloon, compared to all the other (now more boring) prints of it out there. I bet the buyer was delighted.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 7 years ago in reply to shabaz

    According to an article in today's "Sunday Times", the buyer is indeed delighted with the (purely hypothetical, until re-sold) increase in value.

     

    As to earlier comments about the Auction House checking it over, apparently it was "authenticated" by the current Banksy expert and therefore accepted "as seen"

     

    Neil

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • neilk
    neilk over 7 years ago in reply to shabaz

    According to an article in today's "Sunday Times", the buyer is indeed delighted with the (purely hypothetical, until re-sold) increase in value.

     

    As to earlier comments about the Auction House checking it over, apparently it was "authenticated" by the current Banksy expert and therefore accepted "as seen"

     

    Neil

    • Cancel
    • Vote Up +3 Vote Down