Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog Boston Dynamics’ Spot Robot Goes on Sale with Custom Options
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 27 Sep 2019 6:39 PM Date Created
  • Views 2113 views
  • Likes 6 likes
  • Comments 1 comment
  • Boston Dynamics
  • robotics
  • robot
  • cabeatwell
  • spot
  • innovation
Related
Recommended

Boston Dynamics’ Spot Robot Goes on Sale with Custom Options

Catwell
Catwell
27 Sep 2019

image

The Spot base platform features stereo cameras for obstacle avoidance, has a runtime of 90-minutes, and comes with customizable options. (Image credit: Boston Dynamics via YouTube)

 

Boston Dynamics has recently announced they are selling their popular Spot 4-legged robot, which has been in development for years. Annual videos released during that time have highlighted the robots seemingly unnatural capabilities, such as the infamous ‘kicking’ video released back in 2015. The company announced that Spot would be their first commercially available robot at TechCrunch's TC Sessions: Robotics conference last year and they have lived up to their word.

 

Boston Dynamics explains, “Spot is an agile, mobile robot that you can customize for a wide range of applications. The base platform provides rough-terrain mobility, 360-degree obstacle avoidance, and various levels of navigation, remote control, and autonomy. You can customize Spot by adding specialized sensors, software, and other payloads. Early customers are already testing Spot to monitor construction sites, provide remote inspection at gas, oil and power installations, and in public safety. Spot is in mass production and currently shipping to select early adopters.”

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Under the hood, Spot is outfitted with five sensor modules located in the front, back, and both sides, which gives it 3600 awareness of its environment. The legs are driven with 12 reduction motors, giving it a top speed of around 5-feet per-second, and its onboard battery allows the robot to run for 90-minutes before needing a recharge.

 

Along with with the base unit, Spot can also be customized with different hardware configurations, including a 6-DOF arm, and a camera system capable of taking Google Street View-type of images in an indoor setting. There’s no word on pricing, even for the base unit, as there are too many options for its configuration, however according to in an interview with VP of Business Development (Boston Dynamics) Michael Perry from IEEE Spectrum, leasing Spot will be less than the price of a car.

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 7 years ago +2
    This really is a great mobile robot. If I hadn't been watching the videos of it all these years I would never have believed it was possible. There must be some great live action films you could make with…
  • dubbie
    dubbie over 7 years ago

    This really is a great mobile robot. If I hadn't been watching the videos of it all these years I would never have believed it was possible. There must be some great live action films you could make with this.

     

    I wonder if one day they'll make a version big enough ride. With only a 14 kg carrying capabilities I might need quite a few working together to cart me around.

     

    Dubbie