Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog California Startup Comes Up with a New Way to Generate Power with Sunlight at Night
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 3 Sep 2024 6:44 PM Date Created
  • Views 7507 views
  • Likes 4 likes
  • Comments 15 comments
  • hack_the_planet
  • hmi
  • space
  • cabeatwell
  • idea
  • concept
  • service
  • innovation
Related
Recommended

California Startup Comes Up with a New Way to Generate Power with Sunlight at Night

Catwell
Catwell
3 Sep 2024

image

Reflect Orbital tested its concept by fitting mylar mirrors on a hot air balloon that reflected sunlight on a moving truck. (Image Credit: Reflect Orbital)

Fly by night, conceptual, viral, whatever the case may be, this idea is inspiring. It's something that might not have popped into mind could even be possible. That is what we engineers do, alot. Form ideas. Seeing them through is another miracle. 

Reflect Orbital proposed a new, profitable way to boost power generation: selling sunlight after darkness falls. This innovative technique would use satellites to reflect sunlight to the Earth’s surface, potentially lighting up the night sky. Ben Nowack, Reflect Orbital CEO, unveiled this concept at the International Conference on Energy from Space in April. 

Nowack’s idea is based on launching 57 earth-orbiting satellites equipped with 33 sq ft. ultra-reflective mylar mirrors that reflect sunlight onto ground-based solar farms. This means Reflect Orbital could sell sunlight to solar power plants, giving them an extra 30 minutes during peak times. That energy would then be sent to customer’s homes.

The team tested this idea by placing an 8x8 foot mylar mirror on a hot air balloon that reflected sunlight on solar panels attached to a moving truck. It took them a few weeks of fine-tuning before achieving a breakthrough. The mirror reflected light from 242 meters away onto the solar panels that produced 500W of power/square meters of panel. One team member also moved the panels away from direct sunlight, verifying the achievement. Reflect Orbital projections say that energy generation significantly decreased after the panels were moved.

image

(Image Credit: Reflect Orbital)

Although solar power generation is more affordable, it still has some inconsistencies, making widespread adoption challenging as a renewable source. 

Sunlight can also be blocked by thick clouds and stormy weather, affecting solar power generation. Seasonal changes also indicate how much sunlight covers certain regions. Even though the equator receives more sunlight year-round, the north and south hemispheres see a drastic decrease in daytime hours during winter — caused by Earth’s 23.5-degree axial tilt.  

The startup hopes its mirror-equipped satellites can overcome those obstacles by beaming sunlight anywhere on Earth. Russia tested something similar during the late 1980s and early 1990s via the Znamya project. It involved building a satellite fitted with mylar mirrors to reflect sunlight effectively. However, Russian scientists couldn’t replicate that success after the Soviet Union’s fall due to the high cost of launching satellites into orbit at the time. 

Reflect Orbital’s next move involves launching a prototype satellite in 2025 now that its mirrors can boost solar plant’s efficiency. 

Have a story tip? Message me at: http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • DAB
    DAB over 2 years ago in reply to Jan Cumps +1
    Both, the level of light pollution has been getting steadily worse. Creating huge mirrors in orbit would make the situation much worse. If you are beaming meaningful amounts of light to the earth,…
Parents
  • DAB
    DAB over 2 years ago

    As an amateur astronomer I would not be in favor of this system.

    Forget about the energy inefficiencies, the last thing we need is something like this in orbit. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to DAB

     DAB , do you base that on ethical grounds or engineering ones?

    My opinion is based on what I think of this idea as an engineer. As engineer, I think that it has its place in the heads, hearts and phantasy. Not in space.

    It might be a different equation if we had a moon base. And we 'd need more energy there, than the sun can supply by default...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to DAB

     DAB , do you base that on ethical grounds or engineering ones?

    My opinion is based on what I think of this idea as an engineer. As engineer, I think that it has its place in the heads, hearts and phantasy. Not in space.

    It might be a different equation if we had a moon base. And we 'd need more energy there, than the sun can supply by default...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • DAB
    DAB over 2 years ago in reply to Jan Cumps

    Both, the level of light pollution has been getting steadily worse.

    Creating huge mirrors in orbit would make the situation much worse.

    If you are beaming meaningful amounts of light to the earth, you are contributing to warming the atmosphere, plus creating potentially deadly effects if someone takes over control and moves all of that energy to one spot. You could start forest fires, heat islands, and melt snow cap at times that would be very bad for the population.

    Even for a moon base, you still have potential misuse issues that could be very bad.

    I understand the desire for these types of ideas, but when you evaluate them from a risk perspective, they are too dangerous to be built.