Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog Displays, Connectors and Soldering at the Southern Manufacturing and Electronics Show in Farnborough
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 11 Feb 2016 9:11 PM Date Created
  • Views 2470 views
  • Likes 11 likes
  • Comments 16 comments
  • connectors
  • wurth_electronics;
  • wurth;
  • jbc
  • wurth-electronics
  • trip_report
  • wurth_elektronik;
  • soldering
  • pace
  • midas
Related
Recommended

Displays, Connectors and Soldering at the Southern Manufacturing and Electronics Show in Farnborough

shabaz
shabaz
11 Feb 2016

Introduction

The three-day UK Southern Manufacturing and Electronics show in Farnborough’s airfield closed today, and I had the chance to visit it briefly. There were hundreds of exhibitors – from all corners of the UK and beyond. It really made one feel that manufacturing is still alive and well in the UK!

For electronics engineers the show was particularly useful – a great opportunity to see some of the products you might want to incorporate in designs and the types of tools and hardware you might want to use. Aerospace, defence, automotive, medical and contract electronics manufacturing categories were covered. Injection moulding, 3D printing and prototyping, laser cutting and CNC machining and robotics firms were presenting their products too. Probably more than 400 different exhibitor stands on the day I visited. There were also plenty of free to attend seminars (I counted around 30).

 

image

(Image source, cropped and shrunk)

 

Here is an extremely small photo summary from a few of the exhibitors.

 

Midas Displays

Midas Displays had plenty of displays on show. The ones in the photo below (click photo to enlarge) are liquid crystal technology. The upper half of the photo shows ‘VA’ technology displays which are like a low cost alternative to OLED (brighter/sharper than conventional LCD displays, but not as good as OLED in these respects).

image

 

The photo below shows the OLED range. In terms of display lifetime, yellow and green displays last longest. Also the larger the pixel size, the longer the lifetime. There are also sunlight readable displays (provided it is not full-on direct sunlight).

image

 

Wurth Elektronik

Wurth Elektronik had on display some of their product lines too. I liked their connector demonstration PCBs; sometimes it is hard knowing what a connector looks like from datasheets so here are some photos with product numbers mostly visible that can be used as a quick reference. The photo below shows predominantly terminal blocks:

image

 

The red PCB here shows wire-to-board, terminal blocks and some miscellaneous connectors:

image

 

PACE

PACE had their soldering and rework products on display. This very nice workstation uses infra-red heating and a laser aid for visualizing where the infra-red energy will be concentrated (the laser spot is visible on the PCB in this photo):

image

 

There is a very much more affordable hot-air based workstation here, it is in the Farnell catalogue too (would be nice to road-test !)

image

 

Soldering: What Temperature? What Power?

I asked the PACE and JBC guys on optimal soldering iron temperature since I wasn't sure. In their opinion, 330-340 degrees C is about expected for leaded solder, and higher for lead-free solder. Some other bits of advice; use a larger tip if possible for your work, although even 0.4mm tips are possible, something bigger is generally preferred. Don’t drag-solder if you don’t want to; conventional tips and conventional soldering is totally fine if that is what you are comfortable with. Why should you upgrade to a new system? One reason is power related. With a higher power soldering station, you can afford to lower the tip temperature because you have a lot of power in reserve to push heat into your workpiece. So with (say) a capability of 70-80W or so, a 320-330 degree C tip temperature is very feasible for leaded solder. But with 120-130W of power capability the tip temperature can be reduced by a further 10 degrees, down to about 310 degrees C for leaded solder, and no more than 350 degrees C for lead-free solder. The temperature reduction also prolongs the tip life.

The benefit of having immense power was easily demonstrated with a tiny tip and a coin. It was possibly to warm the coin despite the tip being so tiny because of the high amount of dynamic power-on-demand that was available to transfer heat into the coin.

 

Summary

In summary there was lots to see at the show. And you get to see some aircraft since it is right next to the airfield. It is probably worth spending a couple of days at such a show to see all you want to. I will definitely try to visit again next year. (It is free to attend but bring your own food and drinks, that was very pricey!).

This was a very short blog post on the exhibition, I would have loved to do it more justice but unfortunately I was only there for a few hours. But I hope it shows that it would be worth visiting in future because it was great!

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 10 years ago +4
    Very nice presentation. sleuz The photo showing the connectors is a great idea for many catalogues. All too often the graphic shows the particular connector but this presentation is a great idea to see…
  • Problemchild
    Problemchild over 10 years ago in reply to mcb1 +3
    For through hole I've found the cheap pistol grip they do@CPC to be very useful and represents good value @60 ish ...How have you got on with yours? I think a road test for the BGA rework station would…
  • shabaz
    shabaz over 10 years ago in reply to mcb1 +3
    Hi Mark, It was a very cool way to get a view of so many connectors so quickly! The PCB holder is available in a couple of sizes, and combined with the other parts allows for quite precise targeted heat…
Parents
  • jw0752
    jw0752 over 10 years ago

    Hi Shabaz,

    Thanks for the pictures from the show. The information on soldering temps and techniques from the experts are always appreciated.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 10 years ago

    Hi Shabaz,

    Thanks for the pictures from the show. The information on soldering temps and techniques from the experts are always appreciated.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • shabaz
    shabaz over 10 years ago in reply to jw0752

    Hi John,

     

    Thanks! For me also, it was exactly that which I valued greatly - the ability to be able to ask and get back valuable answers immediately!

    Including plenty of useful, informal stuff such as "don't use that part from our product line, this one is better for your needs because xyz" or

    "we sell those parts to a Formula One customer" etc.