Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog EPFL scientists develop an artificial leaf with oxygen production capabilities
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 28 Jun 2021 6:38 PM Date Created
  • Views 1596 views
  • Likes 2 likes
  • Comments 1 comment
  • research
  • manufacturing
  • on_campus
  • cabeatwell
  • biomimicry
  • university
  • solar
  • innovation
Related
Recommended

EPFL scientists develop an artificial leaf with oxygen production capabilities

Catwell
Catwell
28 Jun 2021

image

EPFL scientists demonstrate an artificial leaf that produces oxygen from water, solar energy, and semiconducting polymers. (Image Credit: LMNO/EPFL)

 

Photosynthesis, which isn't efficient for plants, involves converting water and sunlight into oxygen and stored chemical energy. Converting solar energy into chemical fuel at an economical and globally scalable level offers an alternative to fossil fuels. The search for an efficient and affordable artificial photosynthesis process has been a decades-long undertaking. Scientists at EPFL's Laboratory for Molecular Engineering of Optoelectronic Nanomaterials (LIMNO) developed an artificial leaf that uses semiconducting polymers to achieve solar-driven water oxidization. They say these capabilities could pave the way toward solar fuel production.

 

Earlier systems, which weren't industrialized due to low performance and high costs, consisted of inorganic materials like metal oxides or silicon. The artificial leaf's polymeric materials, solution-processed at low temperature, contain molecularly tunable properties. As a result, these can be large-scale manufactured at an affordable cost. 

 

The team reached this achievement by tuning the polymers' properties to equalize the water oxidization reaction requirements. Then, these were assembled into a bulk heterojunction (BJH) blend, allowing a more efficient solar-driven catalytic reaction. Optimizing the device's electronic charge conduction with engineered interfaces also contributed to the water-oxidizing photoanode based on a BHJ polymer blend. This demonstrates higher performance by two orders of magnitude compared to earlier organic-based systems. Additionally, the team discovered crucial factors leading to improved O2 production, which could present new opportunities focusing on more performance improvements.

 

The technique's potential could provide advancements in the polymer-based electronics field. It also presents a pathway toward affordable, efficient, and scalable solar fuel production via artificial photosynthesis.

 

Have a story tip? Message me at: http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • dougw
    dougw over 5 years ago +1
    I don't quite get it. Partly because the explanation is simplified. (I probably wouldn't get it if the explanation was much more complicated either) Photosynthesis (simplified) converts carbon dioxide…
  • dougw
    dougw over 5 years ago

    I don't quite get it. Partly because the explanation is simplified. (I probably wouldn't get it if the explanation was much more complicated either)

    Photosynthesis (simplified) converts carbon dioxide plus water into sugar plus oxygen.

    The process above seems a long way from photosynthesis.

    If it is extracting oxygen from water then there would be a hydrogen by-product and it would be equivalent to electrolysis.

    More efficient electrolysis would be useful, if that is what is going on.

    If it is extracting the oxygen from the polymer, then it would deplete the polymer and use it up.