Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog Open source autonomous driving project to be developed with 96Boards
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 28 Dec 2018 10:44 PM Date Created
  • Views 794 views
  • Likes 4 likes
  • Comments 1 comment
  • research
  • transportation
  • autonomous
  • cabeatwell
  • open source
  • opensource
Related
Recommended

Open source autonomous driving project to be developed with 96Boards

Catwell
Catwell
28 Dec 2018

The Autoware Foundation has been established with collaborations from Linaro, Japan-based company Tier IV and auto-driving software firm Apex.AI. The foundation is an open-source platform for autonomous vehicles based on Tier IV's Linux/ROS Autoware software. The foundation is a non-for-profit organization meant to provide growth, initiate and fund open-sourced projects with Autoware.AI, Autoware.Auto and Autoware.IO.  Autoware.IO will contain platform support based on 96Boards products, vehicle control interfaces and an array of third-party software and hardware tools. The projects include simulators, device drivers for sensors, hardware-independent programs and by-wire controllers for vehicles. Overall, Autoware is in use by over 100 companies in more than 30 vehicles. The bsd-licensed platform accommodates self-driving modules composed of sensing, computing and capabilities that calculate actuations with support specifically designed for camera, LiDAR, IMU and GPS for navigating. 

 

Shinpeo Kato developed the original autonomous vehicle, Autowae.AI. Tier IV was later on founded by Kato to create Autoware.Auto by rewriting Autoware.AI with ROS 2.0. It will run on Tire IV's mini-EV, Milee and Logiee. 

 


A rendered image of Milee, Tier IV's autonomous EV.  (Image Credit: http://linuxgizmos.com/open-source-autonomous-driving-project-to-build-on-96boards-sbcs/)

The autoware is meant to be used for driving under 40mph. Milee and Logiee both run on Autoware.Auto stack on Nvidia's Arm-powered Drive PX2 mainboard for autonomous vehicles. image

 

3D maps and SLAM algorithms enable localization features with GNSS and IMU sensors. Meanwhile, detection algorithms are connected to cameras and LiDARs using deep neural networks and sensor fusion algorithms. The prediction functions are based on localization and detection module outputs. It is available with a simulation environment for users who do not have a Drive PX2 development kit.

 

The connection between Apex and AI isn't very clear. The Palo Alto company offers an autonomous vehicle of Robot Operating System 2.0 named Apex.OS. It's designed to run on Linux while still supporting Windows and QNX.

 

Many open source autonomous driving projects have been created, including the openpilot driving agent. It's the first open source driving stack being used. Other open self-driving platforms have been summarized here, in the TTN story. Linux's open source Automotive Grade Linux in-vehicle project will move into autonomous vehicles at a later date.

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply
Parents
  • jdlui
    jdlui over 7 years ago

    Great to hear that open source collaboration on autonomous vehicles is happening. But why are they speed limited to 40 mph? Simple damage and risk liability?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jdlui
    jdlui over 7 years ago

    Great to hear that open source collaboration on autonomous vehicles is happening. But why are they speed limited to 40 mph? Simple damage and risk liability?