Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog Researchers develop LoCoQuad, an arachnoid-inspired robot
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 9 Apr 2020 8:40 PM Date Created
  • Views 1974 views
  • Likes 5 likes
  • Comments 3 comments
  • research
  • open-source
  • robotics
  • robot
  • github
  • on_campus
  • cabeatwell
  • university
  • innovation
Related
Recommended

Researchers develop LoCoQuad, an arachnoid-inspired robot

Catwell
Catwell
9 Apr 2020

image

The four-legged arachnoid-inspired quadruped robot is capable of walking, turning, swinging, waving and even take pictures. It can be useful in research and education in the future. (Image Credit: Bernal * Civera, YouTube)

Two researchers, Manuel Bernal-Lecina and Javier Civera Sancho, from the University of Zaragoza in Spain, have developed an arachnoid-inspired quadruped robot named LoCoQuad, which could be used in numerous applications for robotics research and education. The team presented their findings in a pre-published paper on arXib. The open-source robot has incredibly low hardware costs, ranging from $150 to $165 USD, and its software and design can be found on GitHub.

 

After conducting research on inexpensive robots and creating several 3-D printed components, Bernal-Lecina began a collaborative effort with Javier Civera to develop a new robot. Their goal was to create an inexpensive robot platform that could serve as a benchmark to train and evaluate state-of-the-art, reinforcement learning algorithms.

 

LoCoQuad is a robotic platform that can walk, turn, wave and even swing by actuating over its four legs. The robot has also been equipped with several sensors, a frontal camera, an inertial measurement unit (IMU) with an accelerometer, gyroscope and two ultrasonic depth sensors. They also use Raspberry Pi as a control unit, which allows the sensors to be flexible and extended.

 

All the sensors and electronics are placed in the main body of the robot. The battery pack is placed on the bottom, power and driver boards are in the center, and the control board and sensors are on the top. This design enables the robot to achieve balance. All four of the robot legs are connected using MG90S servo horns inserted on custom 3D staples. In order to connect each link, the team designed different 3D parts to fit various ranges of motion and a wide range of positions and configurations. In its basic design with two joints per leg (rotator and knee), LoCoQuad contains four different configurations per knee. There are 16 configurations (4 at the elevator and 4 at the knees) in another design, which consists of three joints per leg (rotator, elevator and knee). These different mechanical variations allow the robot to change and adapt to different shapes.

 

The four-legged arachnoid-inspired robotic platform’s low hardware costs could allow it to be easily manufactured on a large scale. Even though it’s not the most efficient quadruped robot to date, the fact that it’s inexpensive, open-source, highly configurable and user friendly, makes it a promising platform for research and education purposes.

 

Both researchers demonstrated the LoCoQuad’s effectiveness in a series of experiments. By doing so, they discovered that it could carry out a wide range of basic tasks, which suggests that the platform could be used in an effort to test out reinforcement learning and different machine-learning algorithms. One of which includes reinforcement learning models, which are being used to develop more efficient and smart robots. LoCoQuad could be used to test these techniques and identify ways for it to be improved.

 

The researchers have already started to use the quadruped robot in other studies to compare different algorithms and identify which ones are most effective. They also hope that LoCoQuad’s design and software will be downloaded by other teams around the world to test out their own machine learning algorithms.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • genebren
    genebren over 6 years ago +1
    Love it!
  • ankur608
    ankur608 over 6 years ago +1
    Almost mimicks like a crab, Great build.
  • dubbie
    dubbie over 6 years ago +1
    A nice robot. Regretfully it suffers from the problems four legged crab like robots have, that they are not very good at moving forwards as they can only lift one leg off the ground at any one time and…
  • dubbie
    dubbie over 6 years ago

    A nice robot. Regretfully it suffers from the problems four legged crab like robots have, that they are not very good at moving forwards as they can only lift one leg off the ground at any one time and have to move the centre of gravity away from the lifted leg in order to avoid falling over. This results in a complicated gait which mainly works by using the front two legs to pull the body forwards like a turtle in quite small increments. Good fun and cheaper to produce though.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ankur608
    ankur608 over 6 years ago

    Almost mimicks like a crab, Great build.image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 6 years ago

    Love it!