Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog Robotics: An Extra Pair Of Hands On The Body
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 19 Oct 2018 6:49 PM Date Created
  • Views 824 views
  • Likes 5 likes
  • Comments 1 comment
  • stem
  • robotics
  • robot
  • on_campus
  • Science Fiction
  • cabeatwell
  • university
Related
Recommended

Robotics: An Extra Pair Of Hands On The Body

Catwell
Catwell
19 Oct 2018

image

It is now possible to have an extra pair of hands on one’s body. A researcher in Japan created a set of hands that can be worn like a backpack. A person wearing the “backpack” with robotic limbs (Image via Yamen Saraiji)

 

According to Merriam Webster, science fiction is the branch of fiction that presents the effects of a real or imagined scientific fact on people or a community. Today, it is kind of hard to know whether fiction is inspiring reality or vice versa. Many situations that used to possible only in sci-fi (science-fiction) books and movies are taking shape in reality. Maybe it is true that if we can imagine something, we can achieve it like Williams Arthur Ward said once upon a time. But, these days reality is catching up fiction at a fast pace. The latest invention inspired by fiction is the additional mechanic and autonomous arms that one can wear, just like the ones Dr. Octopus had in the movie Spiderman. Apparently, the arms are part of a new category of robots called “telepresence robots.”

 

A telepresence robot is a robot controlled by a computer or tablet or smartphone, which permits that 2 parties far apart interacts easily as if they were present in the same. For example, if a person X living in Tokyo has to attend a meeting in Chicago, he or she can use a telepresence robot placed in the meeting room with the other attendees. The robot will display person X on its screen while person X who connects using a smartphone or computer or tablet, can see the attendees of the meeting and interact with them as if he or she were there. In other words, person X will be “remotely present” at the meeting.

 

Telepresence robots are even called “Skype on wheels.” Some might argue that it is not necessary if the participants of a meeting all plug in using a tool such as “Zoom” or even Skype, but such tools don’t offer the flexibility the robot does. For example, some telepresence robots have a laser pointer allowing the operator to give a full presentation looking back and forth between a screen and the audience. The operator of a telepresence robot can also move around in the meeting room and interact individually with other attendees if necessary.

 

Now using the same concept, Yamen Saraiji, an assistant professor in Media and Design at Keio University, came up with a set of artificial arms that can be worn like a backpack and controlled remotely by another person; as in getting an extra pair of hands from someone who is not in the same room as the wearer. The “backpack” consists of 2 moving robotic hands and a robot’s head that hangs over the shoulder of the wearer. To control the hands remotely, the operator uses Oculus Rift and a touch device. The robot’s head has 2 cameras that also allows the remote operator to see what the “backpack” wearer sees. Even though the idea is just a concept for now, it is very promising.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

With this, it is not just fiction that is becoming a reality, but one of mankind’s dreams is coming to life. Everyone can use a helping hand from time to time, but distance is often an obstacle. However, if this robotic arm is fully developed, it will solve a lot of challenges. People with a handicap can certainly use it, and so can rescuers. Even the military might find it useful. The question now is “what is keeping the Saraiji from developing and selling it?”

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • genebren
    genebren over 7 years ago +2
    So cool! I am so right hand dominate that I barely use my left hand for more than a counter balance. If I had more hands, I am not sure if they would be helpful.
  • genebren
    genebren over 7 years ago

    So cool!  I am so right hand dominate that I barely use my left hand for more than a counter balance.  If I had more hands, I am not sure if they would be helpful.