Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog SoFi The New Robotic Fish In The Ocean
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 7 Aug 2018 3:19 PM Date Created
  • Views 1648 views
  • Likes 5 likes
  • Comments 5 comments
  • mit
  • robotics
  • robot
  • on_campus
  • cabeatwell
  • university
  • innovation
Related
Recommended

SoFi The New Robotic Fish In The Ocean

Catwell
Catwell
7 Aug 2018

image

MIT researchers created a robotic fish to facilitate ocean exploration. The new robot can also be a pioneer in biomimetics. Close view of SoFi swimming. (Image via MIT)

 

Mankind has explored many areas of the planet Earth to the point that it could feel as if everything that exists has been discovered. Now, there is a race to explore other planets and galaxies, and that alone spikes a lot of conversations and theories. However, there is a place on planet Earth that still holds a lot of mysteries, a part of the planet that can reshape continents and countries: the oceans. It probably sounds unbelievable that humans have not discovered everything about the oceans yet. To be precise, only five percent of the oceans has been mapped, and one would think that since oceans represent 70 percent of the surface of the planet, humans should get to know them as much as possible. It is an illusion to think that because we have been navigating the oceans for centuries, we have them figured out. The challenge resides in the technology to use for that exploration.

 

First, after 200 meters, it becomes hard for humans or machines to see anything. In addition, the pressure of the water increases the deeper one goes. To top it off, oceans are so vast that it is estimated that 99 percent of livable space is under the oceans. So how to overcome these challenges. Probably by focusing more on developing the right kind of technology. And, that must be the goal of MIT researchers when they created SoFi, the Soft robotic Fish.

 

The researchers explained that they created SoFi because they realized that overfishing was decreasing the population of fish they thought they had to do something to study the ocean life while there is still time. Not the motivation one may expect, but it is still somewhat noble. The truth is that it can be difficult for humans to observe fish, so the scientists imagined that they should let another fish, even a fake one, do the observing for them. Joseph DelPreto, one of the authors of the robot, explained that the robot was designed in a way that it would not obstruct or disturb the natural habitat and the habits of the real fishes.

 

Contrary to many of the robots, mankind has sent in the oceans as explorers, SoFi is not just a machine. Inspired by tuna, jellyfish and lobster, SoFi can swim like a fish by sweeping its tail left and right. And, the fact that the skin of the robot is made of silicon elastomer surely facilitate the movement. The movement of the tail is controlled by a hydraulic mechanism and allows the robot to swim at various depths. SoFi’s head carries a Linus PC along with a camera that serves as its eyes. Even though the robotic fish is quite independent, there is still a remote that allows a diver to control the fish when necessary using ultrasonic signals to communicate with SoFi. But SoFi is not famous just for its design.

 

The technology that allows SoFi to behave like a real fish is called biomimetics and SoFi is the very first finished product of such science. In other words, while SoFi will be helping marine biologists study the oceans, it could inspire scientists in other areas of robotics as well. Therefore, opening doors that were closed so far.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • rsc
    rsc over 8 years ago +3
    The ones we had on the ship last month were called "Ocean Gliders" http://auvac.org/uploads/tiny_mce_uploads/ocean_glider.jpg Scott
  • genebren
    genebren over 8 years ago +2
    Wow! That is an awesome robotic fish. Gene
  • 14rhb
    14rhb over 8 years ago +2
    Another great article, thanks Catwell although I'm not too sure what is meant by "99% of livable space is under the oceans". Do you think that refers to aquatic life e.g. the other 1% is rivers and lakes…
Parents
  • genebren
    genebren over 8 years ago

    Wow! That is an awesome robotic fish.

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 8 years ago

    Wow! That is an awesome robotic fish.

    Gene