Industrial Automation
  • Technologies
  • More
Industrial Automation
Blog Sweating robot alerts when it’s too hot
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Industrial Automation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 3 Jul 2020 6:20 PM Date Created
  • Views 900 views
  • Likes 5 likes
  • Comments 1 comment
  • research
  • japan
  • cool
  • robotics
  • robot
  • on_campus
  • cabeatwell
  • university
  • innovation
Related
Recommended

Sweating robot alerts when it’s too hot

Catwell
Catwell
3 Jul 2020

image

The robot is capable of sweating in high-temperature environments, which can be useful for the elderly. (Image Credit: University of Tsukuba)

 

I think we need sweaty robots. Older people are more prone to suffering from higher environmental temperatures, which can cause a number of serious health issues without warning. Now, researchers from the University of Tsukuba in Japan have developed a robot that alerts them by sweating when the temperature increases. Whenever we get too hot, our bodies produce sweat to regulate temperatures, which is also a feature being used by the robots to convey the impression to the user.

 

Compared to other environmental temperature indicators, including sound or body movement, a sweating robot has two unique benefits. They include a cross-cultural indication where humans sweat despite their region, gender, or culture. The other is an unobtrusive indication that uses peripheral gestures instead of conventional notifications to alert the user about unexpected occurrences through subtle changes. A robot using peripheral gestures is more effective because it indicates increasing temperatures more vividly.

 


The internal design of the robot shows how it can sweat. (Image Credit: University of Tsukuba)
image

In their prototype, the sweating system consists of two modules: pumping modules and gland modules. In the pumping modules, the peristaltic pump is used to draw out the sweat-mimic liquid with different viscosities from the two tanks, which are fixed inside the robot. Afterward, they are mixed and contained within a tube fitted in a pump casing. Then the sweat is transferred through the compression inside a roller station and thus, creates a pulse. This allowed the robot to simulate the sweating process and change viscosity. In the gland modules, the second phase of sweating is simulated. It contains 4mm-diameter tubes that transport the sweat from the pumping modules to the glands. From there, the eight micro solenoid valves that are placed near the robot’s surface will handle the sweat secretion, which will then control the sweating location.

 

In the future, the team plans on carrying out experiments, and afterward, they will upgrade the prototype by adding visual and olfactory effects. They will carry another experiment to identify the benefits of sweating robot indications while comparing it with traditional indication like a thermometer and a verbal alarm. Additionally, the team could add some social aspects to the robot. For example, it could perceive human emotions like nervousness or embarrassment from their sweat and facial expressions. However, it’s not exactly clear if humans could associate the emotional states of a robot with its sweating. In the future, they will also explore sweat as one type of notification of emotion.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 6 years ago +1
    A nice little machine and well enclosed with a good user interface. I'm not entirely sure it is useful. I'm not a fan of excessive heat and tend to sweat myself but I can tell this as I get hot and sweat…
Parents
  • dubbie
    dubbie over 6 years ago

    A nice little machine and well enclosed with a good user interface. I'm not entirely sure it is useful. I'm not a fan of excessive heat and tend to sweat myself but I can tell this as I get hot and sweat - not sure what benefit a robot that does the same would bring. You can get the same information from a combination of temperature sensor and humidity sensor and if outside, a wind speed sensor as well. I use my Alexa to give me this information before deciding on what walk to take, how long for and what clothes to wear. Alexa also tells the time.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 6 years ago

    A nice little machine and well enclosed with a good user interface. I'm not entirely sure it is useful. I'm not a fan of excessive heat and tend to sweat myself but I can tell this as I get hot and sweat - not sure what benefit a robot that does the same would bring. You can get the same information from a combination of temperature sensor and humidity sensor and if outside, a wind speed sensor as well. I use my Alexa to give me this information before deciding on what walk to take, how long for and what clothes to wear. Alexa also tells the time.

     

    Dubbie