• Products and Partners
    Products and Partners
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
Internet of Things
  • Technologies
  • More
Internet of Things
Blog Amazon Echo Dot 2nd Gen Teardown
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 23 Jul 2018 10:22 PM Date Created
  • Views 9177 views
  • Likes 13 likes
  • Comments 7 comments
  • Amazon Echo
  • echo dot
  • amazon alexa
  • amazon
  • amazon echo dot
  • teardown
Related
Recommended

Amazon Echo Dot 2nd Gen Teardown

shabaz
shabaz
23 Jul 2018

This is a teardown of a second-generation Amazon Echo Dot (purchased around January 2017, UK). The photos are fairly high-res and can be clicked to enlarge.

There is a lot of intricate detail in the design.

 image

 

The underside has a peeling part before the self-tap screws can be removed.

image

 

Almost the entire unit comes out, but there is still some stuff in the black plastic shell : ) Notice the two metal contacts for the speaker.

image

 

What the unit looks like outside of its shell.

image

 

The speaker unit can be extracted. The side that was hidden from view is now visible, and you can see the speaker grille too (it's where the arrow is pointing), and there are small holes for it in the outer shell too as you can see. Also notice the radio tag stuck inside.

image

 

Closeup of the speaker unit:

image

The top removed. Now the buttons are visible. The array of holes all around the unit are for the microphones. The are six mics around the circumference, you can see the holes for them in the foam shaped pad. There is also a center microphone.

image

 

The other side; this is the underside of the main control board. That flat flex has a black piece that flips up to open it, easy to miss and damage while removing it : (

The PCB antennas are visible here too, near the top and bottom of the photo:

image

 

The main PCB removed. There is a SIL-PAD type thing for thermal transfer, and two pads for presumably electrical contact to the metal chassis for shielding.

image

 

The metal chassis portion of it can be removed from the black plastic:

image

The top PCB is removed here too, and the underside of it can be seen. The white plastic acts as a light diffuser for the ring of LEDs.

image

 

The plastic removed from the top PCB. Now the microphones and LEDs can be seen.

image

 

Closeup of the two boards:

image

 

Closeup of the top board, microphone soldered side (the buttons and holes for the mics are on the other side).

image

 

The top facing side of the top board:

image

 

The main processor board:

image

Other side of the main processor board:

image

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 8 years ago in reply to jkutzsch +7
    Hi John, Thanks! No I killed it : ( I was defeated by the flat flex, from memory it doesn't stay in place any more although I could possibly hold it in place with tape or something. I had not realized…
  • jkutzsch
    jkutzsch over 8 years ago +5
    shabaz Nice write up. I haven't "acquired" any of those yet for disection! :-) Were you able to get it to work after disassembly? Worse case you may be able to put the innards in a new shell for a different…
  • 14rhb
    14rhb over 8 years ago in reply to shabaz +3
    Hi Shabaz, As I read your article I was thinking about making a comment at the end, regarding "I dislike those little fiddly connectors"...and you seem to have reinforced my opinion. When I did this roadtest…
  • shabaz
    shabaz over 8 years ago in reply to jkutzsch

    Hi John,

     

    Thanks! No I killed it : ( I was defeated by the flat flex, from memory it doesn't stay in place any more although I could possibly hold it in place with tape or something. I had not realized the black part lifted, and I pulled the cable way too hard.

     

    I didn't throw it out though, I kept it in case I wanted to refer to it again, lots of nice design ideas inside there and the PCB antennas looked very interesting too, but I was particularly interested in what they had done with the audio. Also it was quite interesting how many layers of PCB, plastic and metal they neatly sandwiched into the 1-inch or so height!

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jkutzsch
    jkutzsch over 8 years ago

    shabaz Nice write up.  I haven't "acquired" any of those yet for disection!  :-)

     

    Were you able to get it to work after disassembly?  Worse case you may be able to put the innards in a new shell for a different approach to Amazon device.  :-)

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
<