Internet of Things
  • Technologies
  • More
Internet of Things
Forum Success connecting to Arduino Cloud / TTN with MKR WAN 13x0: share your experience (solved)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Internet of Things to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 33 replies
  • Subscribers 518 subscribers
  • Views 12809 views
  • Users 0 members are here
  • ttn
  • cloud services
  • arduino
Related

Success connecting to Arduino Cloud / TTN with MKR WAN 13x0: share your experience (solved)

Jan Cumps
Jan Cumps over 4 years ago

update: solved - it was the coverage.

If you have been successful with sending data to The Things Network / Arduino Cloud, using an Arduino MKR WAN 1300 or 1310, please share your experience.

skruglewicz and I have tried this. The configuration worked for both of us (Arduino Cloud, TTN, customised sketch upload), but we don't get an active sub-1 GHz connection.

If you were able to exchange data, please share where you tried this, what Arduino/antenna combination, and where you placed your gizmo. And if you want, the sketch you uploaded (remove the Arduino-generated ID from the header comments).

Thank you

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 4 years ago in reply to javagoza +5
    Success! Walking tour, and in RED where I had coverage: edit: data also arrived at the Arduino cloud, as expected:
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Jan Cumps +5
    touristic info: the walk was partly through the Louis Bertrandlaan. One of the prettiest lanes of the Brussels district. It's a protected view since 2020. source: https://www.bruxellesbavard.be/nl…
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to shabaz +4
    Has your MKR board worked for any non-LoRaWAN communication, e.g. just plain LoRa? I suppose it could be a faulty MKR board. Yes they are functional. I have two MKR WAN 1310s, and they can perfectly…
  • dougw
    dougw over 4 years ago

    Presumably you have a TTN gateway in range.

    Have you done the process as indicated in this blog?

    https://www.hackster.io/146376/mkr-wan-1310-meets-the-things-network-fff013

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to dougw

    In my case, the coverage is expected to be excellent. 10 active gateways cover my house. skruglewicz has less coverage.

    image

    We used the official howto of Arduino.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • skruglewicz
    skruglewicz over 4 years ago

    In my case, the coverage is pretty weak. 

    But I'm still trying to connect..to the 2 in my vicinity by driving by until i get a signal. I'd be interested in finding out the success of others

    imageimage

    Hope everyone is doing good out there.

    Regards.

    Steve K

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mp2100
    mp2100 over 4 years ago in reply to dougw

    That looks like a good detailed instruction for the arduino cloud portion.  But it's from 2019, and TTN has made changes to their console, bumped the software version up to v3, so you have to check the details.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to mp2100

    In the case of skruglewicz and me, we did not follow the instructions dougw mentioned.

    We used https://docs.arduino.cc/cloud/iot-cloud/tutorials/cloud-lora-getting-started#step-2-registering-the-things-stack-network-account
    These instructions are fresh from earlier this month.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mp2100
    mp2100 over 4 years ago in reply to skruglewicz

    Just guessing from the map, the distance to the closest gateway is ~ 7 or 8 miles?  That's a stretch for LoRa, but possible.  If there is clear line-of-site it could work.  You wouldn't happen to be at the top of a hill?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • skruglewicz
    skruglewicz over 4 years ago in reply to mp2100

    Hello mp2100, CC: Jan Cumps 

    Thanks for the feedback,

    it might be 7-8 miles as the crow flies, but I have hills all around me. 

    I actually have NOT successfully connected to the TTN yet. I tried to but never was successful. I'm just finishing up on a five blog series for an  E14 Design Challenge. The five Blog Series Case Enclosure Reliability Monitor , supplied 2 LoRaWAN Arduino MKR WAN 1300..'s. When I followed the same tutorial described by member Jan Cumps in his comment,  at the time, I suspected, it was a distance issue and I abandoned the connection to the TTN and came up with a new design involving the 2  MKRWAN 1300 as a Sender and Receiver. The New Design was implemented and is working great. I plan to revisit the TTN tutorial soon, maybe this week. 

    E14 Member Jan Cumps ,whom initiated this blog, has excellent coverage and followed the same tutorial as I did for my 1st design attempt. He, as far as I can see,  has NOT successfully connected  to the TTN , as he mentioned above " we don't get an active sub-1 GHz connection."

    So I'm proposing to the Community.  Some questions still remaining are:

    • why can't Jan get an active sub-1 GHZ connection? 
    • He has more coverage than me and he still cannot connect, using the tutorial.?
    • Is there something missing in the tutorial part with TTN configuration?
    • Is he out of range of the 10 gateways on the TTN map?
    • Does any member know of an Arduino sketch that successfully connects to a gateway on the TTN map/
      • Like a TTN gateway range finder

    Kind Regards,

    Steve K

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 4 years ago

    Hi Jan,

    What is in thingProperties.h? I can't see from the user docs where it suggests what to type in there, I may have missed it. Is that the only config file, or any other config elsewhere too?

    Could you paste it (with any sensitive stuff removed), in case anything can be spotted?

    Also, is it  just one order code for the MKR WAN, for both 868 and 915 MHz? Arduino, and Murata site is silent on that.. according to the schematic, the MKR board uses Murata CMWX1ZZABZ which uses the Semtech SX1276 chip, and I was wondering how they matched it to both 915 and 868 MHz, usually such wideband matching would require a more expensive design than if they just had two separate order codes for US and EU. 

    It could be worth buying a low-cost ready-made LoRaWAN device for your region band, just to be 100% sure that it is a MKR issue and not a coverage issue (as you say, coverage should be very good where you are according to what you mention). There are Dragino LoRaWAN sensors, they are reasonable price, and I've confirmed they work with TTN (it is 868 MHz in UK), maybe only slightly more expensive than the MKR, I've not checked prices.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to shabaz

    There are the properties and secret files:

    What is in thingProperties.h? I can't see from the user docs where it suggests what to type in there, I may have missed it. Is that the only config file, or any other config elsewhere too?

    These files are automatically generated by Arduino Cloud, based on things you answer in the Thing Creation Wizard, and partly by values that The Arduino registry process retrieves from TTN while completing that same wizard:

    Properties has, next to the variable I created, also the frequency. I selected the Europe range:

    image

    Secrets contain the keys that are relevant to connect to the correct app (geberated by Arduino when creating the first thing) on TTN

    image

    It could be worth buying a low-cost ready-made LoRaWAN device for your region band, just to be 100% sure that it is a MKR issue and not a coverage issue .

    Yes. I haven' made up my mind yet if I'll use TTN. This was a first attempt to evaluate.
    I'm actually looking for a solution that connects to AWS or Azure Cloud.

    Possibly with my own gateway. I have one currently that I can integrate of the internet with both AWS and Azure.
    And that supports BLE sensors.
    I could try to add sub-1 GHz / LoraWAN sensor collection.

    What I would not get is the coverage outside my own gateway's reach then.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to Jan Cumps

    I see.. I didn't realize you were provisioning from an Arduino portal. I looked at the documentation a bit more, and it suggests you have access to the TTN portal too. What does the device config look like, if you can check it on the TTN portal? There's only a few fields there, I guess you have already checked them out, if you have access. Otherwise if you're not sure of any field but if you have access to that TTN portal, if you can paste a screenshot of that, I can take a look if you like, however I'm sure you would examine it to a high standard anyway.

    Maybe there is a slim chance the firmware on that Murata CMWX1ZZABZ  could need upgrading. There was some code here that displays the version:

    https://www.arduino.cc/en/Reference/MKRWANVersion

    But, also, the code there looks like it is for a generic LoRaWAN configuration, i.e. it could allow you to directly configure in TTN, and bypass the Arduino portal configuration, in case there is something weird going on between Arduino cloud and TTN cloud. Seems a long shot though.. but I guess eliminates one component (the Arduino cloud) just to reduce the possible things that could be causing this.

    It is also possible to confirm transmissions are being sent, and see if the band selection is functioning, this is possible with a RTL-SDR dongle (any cheap one will do, I am using one so cheap the USB connector barely works, it has to be pushed in just right. However they have gone up in price over the years, the typical price nowadays is maybe 25-30 Euro, but they used to cost half this) and SDR Sharp software. This is what it looks like when a Dragino device sends a packet, it is the wide mark indicated with the green arrow (not the narrower width one indicated with red arrow). The frequency will change, but it's possible to set up a wide span like this in order to spot it.

    image

    When the network is joined, there is more data transfer, as shown here:

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
>