Medical
  • Technologies
  • More
Medical
Forum Ultrasound: 1,2,3Mz @ 1,2,3W/cm^2
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Medical to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 15 subscribers
  • Views 425 views
  • Users 0 members are here
Related

Ultrasound: 1,2,3Mz @ 1,2,3W/cm^2

e14 Contributor
e14 Contributor over 15 years ago

Learned colleagues, your input here would be highly appreciated!

 

When applying Therapeutic Ultrasound to a patient's skin surface, at say for example at 2MHz, and at 2W per cm^2,

what is the actual amount of accompanying electrical energy required to generate such sound wave?

Kindly advise an estimated electro-magneteic frequency emission for same, if known?

 

What would be the figures for -

 

  • 1MHz, 1W/cm^2, then 1MHz, 2W/cm^2, and 1MHz, 3W/cm^2

 

  • 2MHz, 1W/cm^2, then 2MHz, 2W/cm^2, and 2MHz, 3W/cm^2

 

  • 3MHz, 1W/cm^2, then 3MHz, 2W/cm^2, and 3MHz, 3W/cm^2

 

I want to study the 'potential' of penetrative ability of the wave(s), at the same time I wish to discover the accompanying

EMFs.

 

Cheers everyone,

 

Rich

=

  • Sign in to reply
  • Cancel
  • Catwell
    0 Catwell over 14 years ago

    Richard,

     

    This reminds me of "Ultrasonic skin tightening." Start there.

     

    Cabe