Medical
  • Technologies
  • More
Medical
Forum 未来5年成像诊断设备市场增长如何
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Medical to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 14 subscribers
  • Views 199 views
  • Users 0 members are here
  • 成像
  • 医疗设备
Related

未来5年成像诊断设备市场增长如何

启蒙19
启蒙19 over 15 years ago

据中国医疗器械行业协会,全球癌症发病率及死亡人数的不断上升,以及癌症发病率逐渐年轻化,推动全球成像诊断设备市场不断扩大。GlobalData研究机构不久前作出预测:作为成像诊断设备的主要产品,X线系统虽然技术创新趋于停滞,但在一些新兴经济体国家,如中国、印度和巴西,仍有较大的市场需求。另外,全球超声设备市场将随技术的发展而不断扩大。未来5年,全球成像诊断设备市场增长的主要驱动力就来自于超声设备的需求。


超声设备市场年均增速7.2%


超声设备的技术已经发展得比较成熟,在2001~2008年间,全球超声诊断设备市场以年均5.2%的速度增长。高速增长的主要原因是全球医疗机构对超声诊断设备的需求不断扩大。另外,超声设备相对于其他成像诊断设备而言成本更低,很多小型医疗机构都具备购买能力。


GlobalData研究机构预测,随着超声系统呈现产品多样化,如出现了便携式设备等,以及应用技术的不断发展,在乳腺癌、宫颈癌、心血管疾病临床检测需求的推动下,全球超声诊断设备市场将以年均7.2%的速度增长,2015年将达到52亿美元的规模。


乳腺X线设备市场年均增速6.9%


从超声、伽马成像到核磁共振(MRI)成像,几乎所有的成像技术都能对乳腺进行检测,但是目前这些成像系统的乳腺成像工作流程仍不十分成熟,很多成像诊断设备公司都希望进一步开拓和占据这一市场。


相对于超声诊断设备市场来说,近年来,全球乳腺X线检查设备市场年均增长速度要慢一些,为4.1%。然而,据预测,随着乳腺癌发病率的升高以及成像技术的不断发展,未来5年乳腺X线检测设备市场将以年均6.9%的速度增长。


MRI装置市场年均增速6.1%


全球MRI市场在2001~2008年间以年均高于6.6%的速度增长。这类设备市场快速增长的主要原因是MRI成像技术的发展,如3特斯拉MRI面世,以及MRI在多种疾病诊断中的推广应用。然而,因MRI设备使用成本较高,以及全球金融危机对医疗器械行业的影响,GlobalData研究机构预计,全球MRI设备市场增速将略有下降,年均增速为6.1%左右。


专业人士分析认为,目前MRI技术的主要趋势是从1.5特斯拉向3特斯拉的高场强转变。3特斯拉场强的MRI能以更短的时间扫描出分辨率更高的图像。它还能为各类病人(如幽闭恐惧症患者)提供个性化扫描成像方案,从而提高MRI成像系统的应用范围。另外,3特斯拉MRI成像技术的发展还将推动肌肉、骨骼、神经和乳腺的成像研究。但是,3特斯拉MRI成像系统也存在一些固有的缺点,如辐射吸收率(SAR)增加。


因1.5特斯拉和3特斯拉MRI成像系统的优点和缺点不同,所以它们的使用群体也不一样。规模较小的医院和检测中心,从成本与工作时间上考虑,会更多地选择1.5特斯拉的MRI系统;而规模较大的医院和检测中心,因具备雄厚资金和充足的技术人员,会选择配置3特斯拉MRI系统。


另据了解,飞利浦公司推出了可将1.5特斯拉MRI成像系统升级到3特斯拉MRI成像系统的工作模式。这种新模式不仅可大大降低医疗机构的安装成本,同时也会缩短技术人员的学习曲线。


CT系统市场年均增速5.4%


计算机X射线断层扫描(CT)系统市场一直备受关注。随着CT设备的更新换代、CT技术的提升以及应用范围的扩大,越来越多的迹象表明,它将进一步取代一些有创性诊断程序,而成为大多数疾病的诊断手段,尤其是它会很快成为心血管疾病检测中一种成本更低、效果更好的手段,例如用CT替代血管造影技术来检测冠状动脉疾病。GlobalData研究机构预测,全球CT系统市场在未来5年的年均增速将达5.4%。


X线系统市场年均增速4.7%


全球X线系统市场在2001~2008年间的增长速度较超声类设备慢,为3.8%。原因是市场趋向成熟,并且在技术层面上也处于成熟稳定阶段。展望未来,GlobalData研究机构预计,风险投资公司对这一市场的投资将会减少。在技术创新上,较其他类成像诊断设备,这类设备将处于趋于停滞的局面。但在中国、印度和巴西等国家,仍有一定的市场需求。未来5年,全球X线系统市场年均增速将达到4.7%。