Medical
  • Technologies
  • More
Medical
Documents Fast High Precision Eye-Surgery Robot Developed
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Medical to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: squadMCU
  • Date Created: 15 Nov 2011 4:28 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 4:42 AM
  • Views 605 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Fast High Precision Eye-Surgery Robot Developed

Researcher Thijs Meenink at Eindhoven University of Technology (TU/e) has developed a smart eye-surgery robot that allows eye surgeons to operate with increased ease and greater precision on the retina and the vitreous humor of the eye. The system also extends the effective period during which ophthalmologists can carry out these intricate procedures.

Eye operations such as retina repairs or treating a detached retina demands high precision. In most cases surgeons can only carry out these operations for a limited part of their career. "When ophthalmologists start operating they are usually already at an advanced stage in their careers," says Thijs Meenink. "But at a later age it becomes increasingly difficult to perform these intricate procedures." The new system can simply filter-out hand tremors, which significantly increases the effective working period of the ophthalmologist.

The robot consists of a 'master' and a 'slave'. The ophthalmologist remains fully in control, and operates from the master using two joysticks. This master was developed in an earlier PhD project at TU/e by dr.ir. Ron Hendrix. Two robot arms (the 'slave' developed by Meenink) copy the movements of the master and carry out the actual operation. The tiny needle-like instruments on the robot arms have a diameter of only 0.5 millimeter, and include forceps, surgical scissors and drains. The robot is designed such that the point at which the needle enters the eye is always at the same location, to prevent damage to the delicate eye structures.

Both slave and master are ready for use, and Meenink intends to optimize them in the near future. The first surgery on humans is expected within five years. He also plans to investigate the market opportunities for the robot system. Robotic eye surgery is a new development; eye surgery robots are not yet available on the market.
 
http://images.sciencedaily.com/2011/10/111027082753-large.jpg
 
Interesting? Read the complete entry
  • precision
  • eye-surgery
  • robot
  • retina
  • surgeons
  • medical