Medical
  • Technologies
  • More
Medical
Documents Ultrasound for Mind Reading
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Medical to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: squadMCU
  • Date Created: 7 Dec 2011 9:23 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 4:45 AM
  • Views 892 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Ultrasound for Mind Reading

Ultrasound is good for more than monitoring fetuses and identifying heart defects. According to engineers in Canada, it can help tell what people are thinking as well. Their research suggests that ultrasound-based devices could lead to a new kind of brain-computer interface.

Brain-computer interface technology allows users to control devices with brain activity alone. Researchers have focused primarily on clinical applications for people with severe disabilities who would otherwise have difficulty interacting with the outside world. In addition to brain-computer interfaces that involve electronics inserted directly into a patient’s head, researchers are also developing a number of noninvasive methods. For instance, electroencephalography (EEG) relies on electrodes attached to a person’s head; functional magnetic resonance imaging (fMRI) uses powerful magnetic fields to measure blood flow in the brain that telegraphs brain activity; magnetoencephalography (MEG) detects the magnetic fields generated by clusters of thousands of neurons; and near-infrared spectroscopy (NIRS) uses light to scan for changes in blood hemoglobin concentrations. Yet practical use of these methods has so far been limited due to a number of drawbacks. For instance, EEG faces "noise" from electrical signals sent by the muscles and eyes; fMRI and MEG are very expensive and require large equipment; and NIRS, while still early in development as a brain-computer interface technology, has a low data-transmission rate. Now biomedical engineer Tom Chau and his colleagues at the University of Toronto reveal that ultrasound can also monitor brain activity, suggesting that it could be used for brain-computer interfaces.

The researchers used lightweight ultrasound headgear to measure blood flow in the brains of nine able-bodied adults as they alternated between relaxing and performing two mental tasks. One task required them to think of words that began with a letter displayed on a video screen, and the other asked them to compare two objects rotated to different angles and determine whether they were the same object or mirror images of each other. Using this new technique, researchers could see with 82.9 percent accuracy whether people were performing the word-generation task and they could tell with 85.7 percent accuracy if they were doing the mental-rotation tasks or just relaxing. Word generation usually led to an increase in blood flow in the left middle cerebral artery, while mental rotation caused increases in both the left and right middle cerebral arteries.
 
http://pre.cloudfront.goodinc.com/posts/full_1307051888Brain-Games-at-Lumosity.jpg
 
 
Interesting? Keep reading
  • ultrasound
  • monitoring
  • eeg
  • medical
  • brain
  • fmri