Motors and Drives
  • Technologies
  • More
Motors and Drives
Forum Soft Starters vs VSD
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Motors and Drives to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 74 subscribers
  • Views 449 views
  • Users 0 members are here
  • 2-phase_control
  • 3-phase
  • motor_starters
  • soft_starters
  • cost_saving
  • fairford_electronics
  • induction_motors
  • motor
  • fairford_energy
  • energy_saving
Related

Soft Starters vs VSD

e14 Contributor
e14 Contributor over 15 years ago

Fairford Electronics is asked the question on a almost daily basis, "why do i need a soft starter when i can use a drive?"

 

The answer is simple, soft starters are the perfect choice for starting a motor that only works at one speed whereas VSD are the only choice when the user needs to run at a variable speed.

 

Many of the worlds motors run at a fixed speed so dont need the increased cost and features that a VSD brings, almost every factory or installation will have the need for both soft starters and VSD, the key is to select the right tool for the job.

 

The energy saving features of VSD's are good when the motor can be slowed down (pumps and fans) but if the application must run at the designed speed then VSD's cannot save any energy. Fairford energy saving soft starters can save energy on fixed speed applications (that work at a light or variable load) without changing the amount of work that the motor is doing.

 

Please see the attached example of the energy savings that can be achieved by using the Fairford Soft Starters on an application that runs at a fixed speed but at a light load.

Attachments:
imageSD0029302 - Energy Saving Example.pdf