Motors and Drives
  • Technologies
  • More
Motors and Drives
Forum Can a motor controller be seen as a Current controlled source?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Motors and Drives to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 75 subscribers
  • Views 3595 views
  • Users 0 members are here
  • induction_motor
  • matlab
  • motor_controller_model
  • simulink
Related

Can a motor controller be seen as a Current controlled source?

mouch
mouch over 14 years ago

Hi,

 

For a Simulink model I would like to use a very simplified model of a motor controller based on a capacitor and a current controlled source. I am assuming the use of an 3 phase induction motor with motor controller based on a DC to AC inverter.

From what I understand, under regenerative braking the motor generates current which via the inverter  is turned into a DC voltage and current source, which I think can be approached using an Current controlled source and an capacitor.

 

To speed up my simulation, I do not want to simulate the full motor control and motor. I want to assume that the motor and controller can deal with what is expected and that I only see the current and voltages at the DC bus - to which I connect my batteries.

 

To this end, I have calculated the power profile at the bus (as seen by the batteries) based on a drive cycle, vehicle parameters, etc. This powe demand I divide by the voltage I expect at the bus to get the current which I then supply to the current controlled source and capacitor which then get connected to the rest of my model. For example, the battery.

 

My question is:

1. Can a motor controller be seen as a Current controlled source?

2. Are there any oversights I need to take in account if I want to take this approach?

 

Cheers,

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    On the DC bus side, you will need to take into account the internal resistance of the batteries because the supply voltage dips as current increases because of this internal resistance.  When the system is in regen the voltage climbs relative to this internal resistance as well. 

    The regen in most controllers is a side effect of the flyback diode on the switching device the controller will regen unless the IGBT mosfet or whatever actively keeps the potential of the buss close to the potential of the reactively generated voltage.  

    As to treating a motor controller like a current controlled source it would be a very simple simulation.  It would be treating the system like a constant load like a pump, and it could work where if the current commanded falls below a certain point current will flow out of the controller onto the bus.  

    Another thing to take into consideration is the ripple on the DC bus controllers cause by switching lot of amps.  Some component blow fuses for no apparent reason because of this and need inductive reactance added to the input path to bring the ripples to an acceptable level. 

     

    Good luck,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mouch
    mouch over 14 years ago in reply to e14 Contributor

    forrest2192002 wrote:

     

    On the DC bus side, you will need to take into account the internal resistance of the batteries because the supply voltage dips as current increases because of this internal resistance.  When the system is in regen the voltage climbs relative to this internal resistance as well.

     

    So, if there is no battery connected but a super capacitor then the voltage keeps rising (provide the initial voltage of the super cap is at bus level and the voltage level at the controller terminals is higher)?

     

    At the moment I am ignoring ripple from the motor controller, I am just looking at the curretn profile in and out. This is what I need for my simulation.

     

    cheers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 14 years ago in reply to mouch

    I'm finding it very dificult to understand exactly what you are doing  - can you post the model ?

     

    Michael Kellett

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mouch
    mouch over 14 years ago in reply to michaelkellett

    Michael Kellett wrote:

     

    I'm finding it very dificult to understand exactly what you are doing  - can you post the model ?

     

    Michael Kellett

    See attached.

     

    The idea is that for a given drive cycle and vehicle I get a power profile that the bus would see. I can then focus on simulating what a battery and converter need to be able to deal with. And research any problems that might arise.

    The reason for simplifying the motor controller + motor + vehicle parameters is to speed up the simulation time. Simulating converters is already hell in terms of time especially since I want to look at whole drive cycles. As such, any saving in terms of simulation time is good.

     

    Hope this explains it further

     

    cheers

    Attachments:
    imagesimulation.docx
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 14 years ago in reply to mouch

    Hello,

     

    I don't think that the capacitor and the CCS are standard Simulink blocks - can you tell me where they came from ?

     

     

    Michael Kellett

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 14 years ago in reply to mouch

    Hello,

     

    I don't think that the capacitor and the CCS are standard Simulink blocks - can you tell me where they came from ?

     

     

    Michael Kellett

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mouch
    mouch over 14 years ago in reply to michaelkellett

    Thats right they are blocks from the SimPowerSystems toolbox. Which is an expansion to the simulink block set. It allows for simulation using a more electronic approach. I was initially looking to build the whole lot in simulink but then the bi-directional nature of a converter would become problematic. In this case, I can use Simulink for the control strategies while taking a electronic approach to the circtuiry elements.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 14 years ago in reply to mouch

    Hello Dirk,

     

    I'm sorry but I can't really help you with the PowerSystems blockset.

    (I don't have it and I've never used it so I would be shooting in the dark !)

     

    Michael Kellett

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mouch
    mouch over 14 years ago in reply to michaelkellett

    Hi Michael,

     

    I understand. But the question was not about the toolbox, but about whether a motor controller can be seen as a variable current source with a capacitor. I think it can based on a setup of an inverter.

     

    An inverter has basically very little resistor  but with a capacitor in front it can supply high current to the motor (in an induction motor current is the defining factor not so much voltage). Under regen conditions the motor basically becomes a voltage source (l believe the voltage raises as a consequence of the back emf increase). Any current into the capacitor raises the voltage of the capacitor (in my assumptions I am assuming that there are no problems with saturation in the motor).

     

    According to these assumption I should be able to see the motor controller as a variable current source.

     

    Is this more or less correct or are there very large discrepancies in my thinking?

     

    Cheers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 14 years ago in reply to mouch

    Hello Dirk,

     

    I'm unconvinced that you can model the controller this way but it does depend on how you control the current.

    Your capacitor is being charged by a constant current but that means that the power going into the capacitor increases as the voltage across it rises.

    So I think that with the model you have shown me the energy in the cap would increase according to t^2 for constant power from the motor - so the current controlled source is making energy.

     

    I'm not sure - it's all in the blockset - in real life there are no current controlled sources image

     

    Try running the model - do you get sensible results ?

     

    Michael Kellett

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mouch
    mouch over 14 years ago in reply to michaelkellett

    The way I see it under normal conditions:

    The throttle is pressed and the motor controller starts to move the motor (through FOC or whatever). This makes that the motor controller demands a current from the battery (the input to the contrller is a capacitor for some smoothing and voltage measuring).

    So, so far a current controlled source should work. Simulations show a reasonable match to other simulated outcomes in literature.

     

    Under regen conditions (and this is where I am having some doubts, but nothing that realy would stop use of the current controlled source).

    The brake is pressed and assuming that we are not going to recover all the energy but only a part of it. The system is going to react in reverse with current flowing out of the controller. The controller I am using on my dynamometer has an "over voltage under braking" protection which monitors the voltage across the input capacitor and when that goes to high it starts burning of current. In other words,

    So I think that with the model you have shown me the energy in the cap would increase according to t^2 for constant power from the motor - so the current controlled source is making energy.

    The energy that flows into the capacitor is then further transported to -for example- a battery pack.

     

    I got the idea from a paper I read, but under buck (regen) conditions I was encountering some behaviour that I could not explain (was not explained in the paper and I was surprised the author had not made a note on that behaviour). The author connected a buck converter to a bus (with the bus simulated by a curretn controlled source) and only used current control to control the current through the converter. But I found that if the input capacitor isnt monitored the voltage will go sky high or drop to input voltage and the converter will stop functioning. The explanation to this effect is simple: because of the switching behaviour of the converter you do not know exactly how much current you draw out of the capacitor and how much will flow into it. And the tipping point is very steep. i.e. too much current and the capacitor voltage will drop; too little current and the capacitor voltage will keep rising (as per your quote again).

     

    So, all in all, I think it can be done but I wondered why this wasn't reported in the paper. Something I considerd fairly important to the overall functioning.

    My question, here was to find out if more people had looked at this before and if there are serious objections to the use of a current controlled source as a motor controller (in simulation).

     

    cheers,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 14 years ago in reply to mouch

    I'm sorry but I don't think I can help any more   - without seeing the complete model and some actual data I'm just guessing what you are doing.

     

    Michael Kellett

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mouch
    mouch over 14 years ago in reply to michaelkellett

    Lol think I just found my answer:

     

    http://www.dspace.com/en/inc/home/products/hw/simulator_hardware/simulator_specific_hardware/electronic_load_module_30v.cfm

     

    quote:

    It can work as both a current sink and a current source to provide bidirectional current flow, i.e., it generates or consumes real current on ECU motor outputs.

     

    I think this answers my questions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 14 years ago in reply to mouch

    I'm happy if you're happy but the dSpace device is an electronic load intended to simulate a motor not a controller.

     

    Michael Kellett

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mouch
    mouch over 14 years ago in reply to michaelkellett

    True, but what is an inverter but a set of switches that create a path for the current to flow (there is not voltage involved - assuming ideal switches equals no voltage drop). The input capacitor would then see only a sink or a source of current.