Motors and Drives
  • Technologies
  • More
Motors and Drives
Forum DC motor as generator
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Motors and Drives to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 6 answers
  • Subscribers 76 subscribers
  • Views 3633 views
  • Users 0 members are here
  • dc motor
  • electricity
  • brushed motor
  • brushless motor
  • generator
  • power
  • motor
  • glow engine
Related

DC motor as generator

vinceverc
vinceverc over 9 years ago

Hello everyone,
This question might have been asked somewhere else but I was not able to fand any other posts regarding my question, if there are please link them and i will delete this post, so I don't waste anybody's time.

I was recently looking into making a generator. I found some glow engines that don't cost alot (I am on a budget) like this one from ali express (I can also buy from other websites, this one just showed up first): https://www.aliexpress.com/item/GO-Engine-18th-methanol-engine-3-0CC-Without-Glow-Plug-for-1-10-on-road-Buggy/32804111807.html?spm=2114.search0204.3.287.c3ltkE&ws_ab_test=searchweb0_0,searchweb201602_5_10152_10065_10151_10068_5430020_5410020_10304_10307_10137_10060_10302_10155_10154_5370011_10056_10055_10054_10059_100031_10099_5400020_10103_10102_10052_10053_10142_10107_10050_10051_5380020_5390020_10084_10083_10080_10082_10081_10177_10110_10111_5420020_10112_10113_10114_10312_10313_10314_10315_10078_10079_10073,searchweb201603_16,ppcSwitch_5_ppcChannel&btsid=982ac520-824a-4967-816b-8c0d979ee8e4&algo_expid=9ff6c1ab-f534-4c27-94b5-31bdddab7c71-39&algo_pvid=9ff6c1ab-f534-4c27-94b5-31bdddab7c71

 

And I was looking around for a dc motor But I don't know which one to pick. Should i be brushed or brushless? What rpm? what voltage? what amp rating? I heard some motors generate AC and others dc?

I am looking to power something like a buck boost converter to charge 5v things (like phones or camping lights... etc).
Will it provide enough power for these appliances?

 

 

Thanks in advance.

Vince

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +3 suggested
    Hi Vince, If you are doing this project for the fun of building a motorized generator then you should proceed but from your question and description it sounds like you may have a difficult path. A motor…
  • jw0752
    jw0752 over 9 years ago +3 suggested
    Hi Vince, Here is an example of what I am talking about: https://www.amazon.com/PowerPro-56101-Starting-Portable-Generator/dp/B00J261PGQ/ref=sr_1_5?ie=UTF8&qid=1502551377&sr=8-5&keywords=Generator You…
  • dougw
    dougw over 9 years ago +3 suggested
    That is a beast of a motor. It can produce over 1300 Watts which is 91 amps at 14.7 Volts - more than enough to charge anything, including car batteries. It could easily run an alternator from a car or…
Parents
  • jw0752
    0 jw0752 over 9 years ago

    Hi Vince,

     

    Here is an example of what I am talking about:

     

    https://www.amazon.com/PowerPro-56101-Starting-Portable-Generator/dp/B00J261PGQ/ref=sr_1_5?ie=UTF8&qid=1502551377&sr=8-5&keywords=Generator

     

    You can probably find used ones like this for not much more that the cost of the engine you were looking at.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to jw0752

    In past I had one to power the lights when doing out door photo sessions with models. These cheap versions are very bad controlling the fuel engine RPM and consequently the output power is so unstable to broke any kind of device as far as I saw. There are well working ones instead like the CAT devices that costs about 10 times image

     

    By the contrary of what you can imagine, these cheap generators are instead perfect to power battery laptop just because the power does not reach directly the device. If you try to attach a sync flash for photography or a light spot it is a mess.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to jw0752

    In past I had one to power the lights when doing out door photo sessions with models. These cheap versions are very bad controlling the fuel engine RPM and consequently the output power is so unstable to broke any kind of device as far as I saw. There are well working ones instead like the CAT devices that costs about 10 times image

     

    By the contrary of what you can imagine, these cheap generators are instead perfect to power battery laptop just because the power does not reach directly the device. If you try to attach a sync flash for photography or a light spot it is a mess.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 9 years ago in reply to balearicdynamics

    Hi Enrico,

    You make a very good point and it also highlights the likely outcome of building ones own engine motor combo to make a generator. If the inexpensive commercial ones are poorly regulated it is even more likely that a home made combo of hobby engine and motor will be very difficult to regulate and control.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to jw0752

    True John, but I can suggest something that I have discovered casually some years ago. I owned for some years a Honda CBR 600 (the smallest bike I had ever). One day unexpectedly the battery died, so I replaced with a new one and in one day it died too. Before wasting a third battery I informed what was the cause and I discovered that there is a cheap component (about 20 Euro) regulating the power from the generator to avoid damage to the electrical circuit of the bike, in particular the battery overvoltage. A couple of years ago I found this component reused by a a guy to regulate the power of a gasoline generator built by himself. Maybe this is a good starting point to make some tests and research I suppose. These pieces can be found for few $ used as spare parts.

     

    Enrico