Motors and Drives
  • Technologies
  • More
Motors and Drives
Forum 3V Motor Control using Arduino
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Motors and Drives to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 5 answers
  • Subscribers 76 subscribers
  • Views 4596 views
  • Users 0 members are here
  • transistor
  • arduino motor
  • ldr
Related

3V Motor Control using Arduino

ross2609
ross2609 over 8 years ago

I'm not too familiar with Arduino's but I'm very interested to get involved with them as I would like to build my own projects!

 

The circuit that I have built is shown below:

image

 

I am trying to control 3V DC motor using the PWM pins on the Arduino. I'm using an LDR in a voltage divider to provide an analog input into the A0 pin. The code I'm using is provided below:

 

int sensorPin = A0;   // select the input pin for the voltage read from sensor

int motorPin = 9;     // select the pin for the motor

int sensorValue = 0;  // variable to store the value coming from the sensor

int val = 0;

 

void setup() {

  //set the pin mode for the motor to be an output

  pinMode(motorPin, OUTPUT);

  Serial.begin(9600);

}

 

void loop() {

  // read the value from the sensor:

  sensorValue = analogRead(sensorPin);

 

  //Print the value read on A0 into the serial monitor.

  Serial.print(sensorValue);

  Serial.print(' ');

  delay(1000);

 

  //sensorPin ranges between 0 -> 1023 so val ranges between 0 -> 255.

  val = sensorPin/4;

 

  //Motor speed changes relative to the value read at A0.

  analogWrite(motorPin, val);

}

 

THE PROBLEM:

I can't see what is wrong with the circuit but the output voltage from the PWM pin 9 always seems to be roughly 0.05V and the VCC voltage 3.3V is all being dropped across VCE. Therefore I have concluded that there is no current flowing through the transistor.

 

I am not sure how to solve this problem.

 

Thanks for any help!

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +7 verified
    Hi Ross, I've not looked in detail (unfortunately I don't know Arduino so well either), so there could be more issues, but one thing that needs to change is the line: val = sensorPin/4; to: val = sensorValue…
  • jw0752
    jw0752 over 8 years ago +6 suggested
    Hi Ross, I meant to compliment you on the excellent presentation that you made for your question. Good diagrams and background information make responding much easier and more on the point. John
  • mcb1
    mcb1 over 8 years ago +6 suggested
    I agree with jw0752 . It's nice to see ALL the information. Personally I'd drop the series resistor from 660 to 470ohm, or even down to 220. Your calculation for the full collector current shows you need…
Parents
  • mcb1
    0 mcb1 over 8 years ago

    I agree with jw0752. It's nice to see ALL the information.

     

    Personally I'd drop the series resistor from 660 to 470ohm, or even down to 220.

    Your calculation for the full collector current shows you need a 570 ohm and motors always require more current to start.

     

    You may need an external 3v3 regulator or battery to power the motor.

    While the 5v regulator on an Arduino can provide enough, the 3v3 has much less current capability.

     

     

    The sensor to PWM conversion can also be done using MAP.

    https://www.arduino.cc/reference/en/language/functions/math/map/

    It allows some range selection to restrict output, and the example shows reading analogue and driving PWM.

     

     

    Mark

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 8 years ago

    I agree with jw0752. It's nice to see ALL the information.

     

    Personally I'd drop the series resistor from 660 to 470ohm, or even down to 220.

    Your calculation for the full collector current shows you need a 570 ohm and motors always require more current to start.

     

    You may need an external 3v3 regulator or battery to power the motor.

    While the 5v regulator on an Arduino can provide enough, the 3v3 has much less current capability.

     

     

    The sensor to PWM conversion can also be done using MAP.

    https://www.arduino.cc/reference/en/language/functions/math/map/

    It allows some range selection to restrict output, and the example shows reading analogue and driving PWM.

     

     

    Mark

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • ross2609
    0 ross2609 over 8 years ago in reply to mcb1

    Hi,

     

    Thank you very much for your reply as this is very helpful and interesting information! I dropped the resistance down to 470 ohms and the motor has no bother starting up now! The higher current during start up is something I did not consider when designing the circuit so thank you!

     

    Ross

    • Cancel
    • Vote Up +4 Vote Down