Motors and Drives
  • Technologies
  • More
Motors and Drives
Forum What Would You Do with the K4 Drive System Development Kit?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Motors and Drives to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 26 replies
  • Answers 5 answers
  • Subscribers 82 subscribers
  • Views 6919 views
  • Users 0 members are here
  • ebmpapst
  • k4 drive system development kit
Related

What Would You Do with the K4 Drive System Development Kit?

rscasny
rscasny over 6 years ago

Ever so often I get a chance to offer to the element14 community a real jewel of a development kit. I think the K4 Drive System Development Kit by ebm-papst is one of those kinds of kits. Let me tell you a few things about it.

 

Let me start with a picture:

image

Here's what's in the kit:

• K4 Switch Box

• ECI-63.40 or VDC-3-49.15 Motor (-002 and -003 kit versions only)

• RS485 adapter

• RS485 adapter driver download CD

• USB-A to USB-B cable

• RS485 connection wires

 

What can you do with it:

In a nutshell, BLDC motor drive development. You get a motor with gearbox and a switchbox for some serious exploration of this drive system kit.!

 

Here's a few facts about the K4 Switch box:

image

The motor supply terminals are the power input to the motor and the DC to DC converter in the box that generates

24V logic power for the motor’s electronics. Red is positive, black is negative (ground).

• The motor and logic fuses protect the motor from an over current in the event too much power is drawn.

• The motor connector port provides the electrical contact between the Switch Box outputs and the motor inputs.

• The RS485 terminals are the inputs for communication between the motor and a computer via the USB to RS485

adapter included in the kit.

• The readout terminals are meant to allow for monitoring different voltages and provide feedback from the motor.

• The input switches control the digital 24V signals to the motor, which enable and control motor operation. The

switches have 3 positions: Up is toggle-on, middle is off, down is momentary-on.

• The 0-10V analog dial controls the analog voltage signal generated by the Switch Box and read by the motor. This

is usually used as a speed control signal.

 

What would you build with it:

On the serious side, any kind of high performance, position, torque or motor drive application. But, this is element14, let's get creative! Take a look at this cute video and see what one clever engineer did to automate the pouring of his cup of tea. Of course, he used the K4 Drive System Development Kit

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Are you interesting in obtaining this kit?

 

Reply to this discussion and tell me what you would do with it

 

 

P.S. here's the user manual to read and review.

  • Sign in to reply
  • Cancel

Top Replies

  • rscasny
    rscasny over 6 years ago +5 suggested
    Hi All, Thanks for all the great ideas. What's the status of this activity? Well, I wrote the account manager and told her I would like to get some kits for this activity. She is now talking with the sponsor…
  • rsc
    rsc over 6 years ago +4 suggested
    We have a 20 year old mechanism for pulling an object through a fluid for turbulence measurements. The current solution controls motor speed with a manual adjustment that is difficult to control to any…
  • pratyush_cetb
    pratyush_cetb over 6 years ago +3
    During this lockdown, my mother is making a a lot of deserts and the region where I live most of the sweet contain coconut filling inside. I guess building a coconut scrapper with K4 Drive System for my…
Parents
  • rsc
    0 rsc over 6 years ago

    We have a 20 year old mechanism for pulling an object through a fluid for turbulence measurements.

    The current solution controls motor speed with a manual adjustment that is difficult to control to any precision.

    I would replace the current motor and controller with the contents of the kit and attempt to use LabView to automatically control the motor as it takes data.

    Here's a pic of the current motor/drive.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 6 years ago in reply to rsc

    Are you sure you get a gearbox, the two types of motor listed as parts of the kit (I assume you get one or the other) don't include a gearbox.

    From the picture the motor is:ECI-63.40 which comes in 24 or 48 volt versions:

     

    It's a nominal 250W output power motor requiring a power supply capable of 24V, continuous current 12.3A, pk current 36.9A.

     

    It's nice in that the controller is built in.

     

    I mention these things because I don't think that most of the comments above quite get what they will be wrestling with !

     

    If you could persuade Papst to throw in a gearbox it might be quite nice for rsc project -

    (I'm not sure that the motor has enough torque to do his job without a gearbox.)

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rsc
    0 rsc over 6 years ago in reply to michaelkellett

    I’m sure I’ve got a gearbox around that can be used with the kit imageimage

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dubbie
    0 dubbie over 6 years ago in reply to michaelkellett

    Michael,

     

    Ouch! That would be some power supply. I did think after I had put forward an idea what sort of power supply might be needed but then decided I wasn't likely to be successful anyway as it seems unlikely a packet of digestive biscuits would be included so didn't make any amendments. A lack of gearbox might be a more serious limitation.

     

    Dubbie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 6 years ago in reply to dubbie

    If it's the 24V motor a couple of 12V lead acid batteries (sealed from the Grandson) might do.

    The power's about right.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 6 years ago in reply to dubbie

    If it's the 24V motor a couple of 12V lead acid batteries (sealed from the Grandson) might do.

    The power's about right.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • dubbie
    0 dubbie over 6 years ago in reply to michaelkellett

    Michael,

     

    I do have a couple of lead acid 12V batteries (from a fire alarm system) which are OK but I'm not sure they would provide 12A for all that long so I'd be dubious about using them. Suitable lead-acide batterie cost nearer £60 each - I know as once as a lecturer I ran a first year induction exercise to make robot wars robots (full size ones) and we had to buy 20. There was a lot of dark muttering about the cost. Strangely, when I wanted to use them again some time later they had all 'disappeared'!

     

    Dubbie