Motors and Drives
  • Technologies
  • More
Motors and Drives
Forum How cool is this? Electric turbocharger
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Motors and Drives to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 76 subscribers
  • Views 812 views
  • Users 0 members are here
Related

How cool is this? Electric turbocharger

e14 Contributor
e14 Contributor over 16 years ago

Aeristech of Birmingham has secured £500,000 to develop its electromechanical turbocharger.....

 

In a conventional turbocharger, a turbine in the engine's exhaust system extracts power, and delivers it to a compressor through a mechanical shaft. The compressor forces air into the engine....

 

"Turbochargers are fitted to make an engine more powerful by using the energy from exhaust gases, which would otherwise be lost, to raise the pressure of air entering the engine. This also increases engine efficiency and materially enhances fuel consumption," said Aeristech. "However, conventional turbochargers only assist the engine when sufficient exhaust gas energy is available. Any mismatch between what the engine needs and what the turbocharger produces is known as turbo lag."....

 

The answer, according to Aeristech, is to replace the mechanical coupling shaft with a generator, motor, and energy storage device.

These allow the motor to drive the compressor immediately acceleration is required using power from the energy storage device.

Energy is replaced seconds later by the exhaust-driven generator.

 

Complete, original article: http://www.electronicsweekly.com/Articles/2010/06/23/48902/Electric-turbocharger-firm-gets-163500000.htm

  • Sign in to reply
  • Cancel
Parents
  • JohnDSiviter
    0 JohnDSiviter over 16 years ago

    Sounds good, but like all things it all depends how its all put together, Turbos are very simple in design and can operate up to high temperatures, they are now putting a capacitor+motor+generator in there, mm I am sure at least one of those components do not like the heat!, I think it will be pretty tricky building a reliable solution image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • JohnDSiviter
    0 JohnDSiviter over 16 years ago

    Sounds good, but like all things it all depends how its all put together, Turbos are very simple in design and can operate up to high temperatures, they are now putting a capacitor+motor+generator in there, mm I am sure at least one of those components do not like the heat!, I think it will be pretty tricky building a reliable solution image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to JohnDSiviter

    Good points. If I recall my mechanics, most turbochargers require oil pressure to help cool/lubricate them due to 30,000 RPMs to gain the needed PSI.

     

    This heat alone along with engine heat and vibration will be a significant challenge to overcome as you have stated.

     

    One of the interesting points of the article seems to indicate a secondary battery/storage device used at low RPM.

     

    Wonder if its possible to use a new charged capacitor rather than a conventional battery system.