Motors and Drives
  • Technologies
  • More
Motors and Drives
Forum Torque
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Motors and Drives to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 76 subscribers
  • Views 874 views
  • Users 0 members are here
  • robowars
  • torque
Related

Torque

rishi2628
rishi2628 over 11 years ago

I have am dc geared motor like the one below. On the box it is written that it is a 12kgcm torque motor. What does it mean? Does it mean that the motor can carry 12 kg weight with a speed of 1 cm  per second? FYI, I am participating in a robowars competition and i need motors to drive a 60 kg robot.This is my first time and i have no clue how to make a battling bot. So i hope you can give me any suggestion or advice, if possible.Thanks

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • balearicdynamics
    balearicdynamics over 11 years ago +4
    The torque as defined by johnbeetem is correct, I'll try to show you the concept with a couple of images. The short definition of torque in a a DC motor (always we speak of torque also in other rotating…
  • johnbeetem
    johnbeetem over 11 years ago +3
    I took a quick look at the Wikipedia article on torque: https://en.wikipedia.org/wiki/Torque#Units Here's my understanding: Torque has units of force x distance. Think of using a wrench to turn a sticky…
Parents
  • balearicdynamics
    0 balearicdynamics over 11 years ago

    The torque as defined by johnbeetem is correct, I'll try to show you the concept with a couple of images. The short definition of torque in a a DC motor (always we speak of torque also in other rotating shafts mechanical applications) can be the following:

     

    The quantitative measure of the tendency of a force to cause a rotational motion, or to bring about a change in rotational motion

    Please take a look to the following image:

    image

    where R is the angle of the object to be rotated, in the unit definition a 1cm diameter wheel. F is the force that is applied to make it rotating. This applied to the specific case of a DC motor is influenced by the electromagnetic field as shown in the image below (don't matter is the scheme includes the brushes in the motor, I have not found a brushless motor design but it is the same).

    image

    Where, set E as the power supply, Eb is the electromagnetic field the motor is subject to, generating the rotation of the shaft. This express the theoretical torque, while the real value - hopefully what declared by the motor producer - consider the motor resistance to the rotation and the other electromagnetic losses. So in you case, a 12 Kg (that is as far as defined in the previous post by John as the G force on the heart) / cm is the ability of the motor to rotate a mass of 12 Kg applied on a wheel of 1 Cm radius. Based on this reference parameter, as much the wheel diameter is large, as the applied peripheral force to the wheel decreases increasing the angular speed.

     

    Last but not least, please consider that these values are NOT CONSTANT!!!

     

    We can expect that the producer provides a table with the torque and the other DC motor parameters ad certain conditions, like in the following for a generic motor

    image

    That should be accomplished by a curve diagram showing the DC motor efficiency response in different power conditions.

    image

    As these conditions are strongly directly influenced by the power supply respect the nominal power, this is the reason that it is better to control the motors rotational speed with PWM signal pulses instead of a voltage variations.

     

    Enrico

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 11 years ago

    The torque as defined by johnbeetem is correct, I'll try to show you the concept with a couple of images. The short definition of torque in a a DC motor (always we speak of torque also in other rotating shafts mechanical applications) can be the following:

     

    The quantitative measure of the tendency of a force to cause a rotational motion, or to bring about a change in rotational motion

    Please take a look to the following image:

    image

    where R is the angle of the object to be rotated, in the unit definition a 1cm diameter wheel. F is the force that is applied to make it rotating. This applied to the specific case of a DC motor is influenced by the electromagnetic field as shown in the image below (don't matter is the scheme includes the brushes in the motor, I have not found a brushless motor design but it is the same).

    image

    Where, set E as the power supply, Eb is the electromagnetic field the motor is subject to, generating the rotation of the shaft. This express the theoretical torque, while the real value - hopefully what declared by the motor producer - consider the motor resistance to the rotation and the other electromagnetic losses. So in you case, a 12 Kg (that is as far as defined in the previous post by John as the G force on the heart) / cm is the ability of the motor to rotate a mass of 12 Kg applied on a wheel of 1 Cm radius. Based on this reference parameter, as much the wheel diameter is large, as the applied peripheral force to the wheel decreases increasing the angular speed.

     

    Last but not least, please consider that these values are NOT CONSTANT!!!

     

    We can expect that the producer provides a table with the torque and the other DC motor parameters ad certain conditions, like in the following for a generic motor

    image

    That should be accomplished by a curve diagram showing the DC motor efficiency response in different power conditions.

    image

    As these conditions are strongly directly influenced by the power supply respect the nominal power, this is the reason that it is better to control the motors rotational speed with PWM signal pulses instead of a voltage variations.

     

    Enrico

    • Cancel
    • Vote Up +4 Vote Down