Motors and Drives
  • Technologies
  • More
Motors and Drives
Forum Driver Circuit for a Reciprocating Water Pump in a Medical Device
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Motors and Drives to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 31 replies
  • Subscribers 74 subscribers
  • Views 2197 views
  • Users 0 members are here
Related

Driver Circuit for a Reciprocating Water Pump in a Medical Device

jw0752
jw0752 over 1 year ago

Hello Friends,

I am working on servicing a circuit board that is used in a Medical Dental sterilizer. The circuit boards used in this model of sterilizer seem to have a chronic problem with a circuit that drives a reciprocating water pump. Here is a schematic of the circuit that fails:

image

My question is what is the advantage to using this circuit configuaration to drive the pump? The gate of the N CH MOSFET turns on and pulls one leg of the load to the negative rail and also turns on the P CH MOSFET about 20 microseconds later pulling the other leg of the load up to the positive rail. While this seems to work quite well it seems to me to be an added complication to be switching both legs of the load. I am hoping for some insight into what the advantage might be in using this configuaration. The Rds (on) of the N CH is about 60 milli Ohm and the Rds of the P CH is about 13 milli Ohm. While I am not certain this is probably a Pulsed circuit as I suspect that the pump needs a Pulsed drive to properly function. My hope is that in better understanding the advantages of this circuit design I might be able to modify it to lower the present failure rate. Failure is usually a shorted P CH Mosfet, A Heat Destroyed N CH MOSFET and a Shorted D26 Diode.

Any insights you may have will be appreciated.

John

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 1 year ago in reply to jw0752 +2
    Well, the circuit looks a bit weird - I can only think that it has evolved. On similar things I have wanted to protect the load against the low side MOSFET failing short circuit and added a high side…
  • jw0752
    jw0752 over 1 year ago in reply to Jan Cumps +2
    Hi Jan, How have you been? I can't tell you how happy it makes me to see so many of the old gang still together.
  • Jan Cumps
    Jan Cumps over 1 year ago +1
    Is it possible that the fragile gate of G17 sees too much high (inductive generated) voltage, from motor via R103 and R100, when the motor switches off? Maybe hang an isolated scope between drain and gate…
Parents
  • robogary
    0 robogary over 1 year ago

    What's the power source voltage? Is it from a switched supply or a linear regulated ? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 1 year ago in reply to robogary

    This circuit is powered with 24VDC from a linear unregulated power supply.  It is a pretty beefy supply with a 25Amp bridge and an off board transformer.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 1 year ago in reply to robogary

    This circuit is powered with 24VDC from a linear unregulated power supply.  It is a pretty beefy supply with a 25Amp bridge and an off board transformer.