Motors and Drives
  • Technologies
  • More
Motors and Drives
Forum Tower Pro SG90 microservo question.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Motors and Drives to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 75 subscribers
  • Views 1962 views
  • Users 0 members are here
  • servo motor
  • raspberry pi gpio
  • sg90
Related

Tower Pro SG90 microservo question.

sanyika95
sanyika95 over 8 years ago

Hello!

 

I have a question regarding this kind of motors. I am using my Raspberry Pi with the RPi.GPIO library. I have 4 of this motor, I have tested 2 and both of them worked as I write below.

On thier datasheet it is written that I can control them with a signal which frequency is 50Hz and the voltage is around 5V.

Also on the datasheet the -90° rotation needs 1 ms pulse, which would mean that, the duty cycle should be 5%. This works perfectly.

On the datasheet the +90° rotation needs 2 ms pulse, which would mean that, the duty cycle should be 10%. This doesnt works. The +90° rotation is at around 20% duty cycle.

 

This is the datasheet I found: http://www.ee.ic.ac.uk/pcheung/teaching/DE1_EE/stores/sg90_datasheet.pdf

 

Are the motors wrong, or did I understand something badly, or the PWM on the Raspberry Pi is this bad with that library? (I have read something back then it is not the perfect library for motor control)

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +1
    I'm not too surprised. The datasheet for these servos indicates they use pulse widths from 0.5 ms to 2.4 ms to go 180 degrees. I have a couple of these servos and the standard 1-2 ms pulse width doesn…
  • sanyika95
    sanyika95 over 8 years ago in reply to dougw +1
    So the datasheet I found was wrong. Thank you.
  • dougw
    dougw over 8 years ago

    I'm not too surprised. The datasheet for these servos indicates they use pulse widths from 0.5 ms to 2.4 ms to go 180 degrees.

    I have a couple of these servos and the standard 1-2 ms pulse width doesn't give a full 180 degrees.

    https://servodatabase.com/servo/towerpro/sg90

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • sanyika95
    sanyika95 over 8 years ago in reply to dougw

    So the datasheet I found was wrong. Thank you.