Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Blog Free Chemistry, Heating and LoRa stuff [UK]
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 2 Sep 2019 11:16 PM Date Created
  • Views 4278 views
  • Likes 12 likes
  • Comments 23 comments
  • free stuff
Related
Recommended

Free Chemistry, Heating and LoRa stuff [UK]

shabaz
shabaz
2 Sep 2019

Hi, I've got some items unrequired, if you're in the UK and wish to have it, please let me know if you want "chemistry" or "LoRa" or "Heating" stuff and I'll post it for free.

All of this stuff is new and unused, and I hate to just throw it away since it's quite useful stuff.

 

Chemistry stuff:

6 x 100ml beakers (glass), a plastic funnel, 4 glass pipettes and some boxes of universal indicator (like Litmus paper).

 

 

LoRa stuff:

Two SX1276MB1MAS (European variant) LoRa transceiver boards, and two SMA antennas that I think are for the 868MHz band (the boards are dual-band, they have 433MHz capability too with the correct antenna). They're for mbed boards, (might fit Arduino but I don't know), but could easily be connected using jumper wires to any microcontroller board or Pi for instance.

 

 

Heating stuff:

Two Quartz Halogen tubes (277mm long, from Ceramicx, 240V, 1kW each, plus holders with aluminium reflectors and a few miscellaneous things like ceramic screw blocks. I got these with the intent of making a reflow oven, but that never happened.

  • Sign in to reply
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to Jan Cumps

    Data received:

     

    image

     

    Corrupt (CRC error), but It Is Data image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to shabaz

    shabaz  wrote:

     

    ...

    (I cannot see any attachment, maybe it is video still encoding?)

    I've pasted two images from my clipboard. Odd.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to Jan Cumps

    Hi Jan,

    This is awesome!! : ) Glad it is functioning.

    (I cannot see any attachment, maybe it is video still encoding?)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to Jan Cumps

    ... I found out than one of my dev boards, a STM Nucleo, is MBED and has the right headers.

    I used the 868 MHz Ping Pong example, mounted one of the SX1276MB1MAS shields and it worked straight away.

    Below you see a TI CC1310 receiving the Pigs from the Semtech radio.

     

    imageimage

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to Jan Cumps

    ... so I was naively trying to port the MBED libs to "any other device", and I have currently 175 compilation errors.

    I think I'll hold off for a moment and try to create a working port of the libraries for the Project14 all things RF month.

    I can then post about the analysis of the MBED lib, what the MBED specific code is, and how to abstract that.

     

    Not being an MBED user may be the steep part of the curve image. One can but try ...

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>