• Products and Partners
    Products and Partners
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
Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Archaeology Resistivity Meter
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 332 replies
  • Subscribers 332 subscribers
  • Views 56282 views
  • Users 0 members are here
  • armp
  • archaeology resistivity meter
Related

Archaeology Resistivity Meter

kltm
kltm over 6 years ago

Hi I'm looking for ideas on an update to a resistivity meter for archaeology. The only published designs for diy were in 2 magazines. One was published in 1997 and the other in 2003. I have copies of both articles available. The reason behind this is the current high cost of available equipment, usually well beyond the reach of most archaeological groups. I've attached a basic block diagram. In the first magazine article the meter is very basic. It relied on the operators to write down the reading given as the survey was taken. Given that a normal survey grid is 20m x 20m and 1 reading is taken on every sq mtr there would be 400 readings to write down and then input into a program used to interpret the results. The later article is really an update to the first where a PIC has been added to record the readings. This again is prone to error, because eadings are taken manually by pressing a button.

I'm sure given the advances in electronics there must be better ways. 

 

 

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • kltm
    kltm over 6 years ago in reply to michaelkellett +8
    Hi Michael This all sounds very interesting and encouraging. I see you have found the original article, the update is also on slideshare somewhere. I haven’t really thought much about cost, but as you…
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz +7
    I can't live with that - I have to have symmetry The problem is that the Howland current pump doesn't constrain the voltage on the load at all when perfectly balanced - and my LTSpice model is unrealistically…
  • michaelkellett
    michaelkellett over 6 years ago in reply to michaelkellett +7
    AS promised - now for the phase sensitive detector. I couldn't easily model this in LTSpice, which is no great surprise because it needs multiplication and square roots. I used Simulink in MATLAB - which…
Parents
  • robbarter
    robbarter over 6 years ago

    Having started coding my LoraWan custom board using mbed I eventually switched over to CubeIDE.  The mbed environment is confusuing at times especially when creating a custom board for the first time.  It even kept switching my board type occassionally???    You do get a lot of code for free but it needs better documentation especially when creating a custom board.   And as mentioned above, you'll pull in more code than you need.

    My vote at this time (I really want mbed to succeed) is to go the CubeIDE route.  Add in a 6pin SWD connector and you can step through the code line by line in the debugger (I used a Tag-Connect cable. Saves a connector on the board).

    Other people may have better experience.  I've come from a Eclipse env (not great) for LynxOS and Visual Studio.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • robbarter
    robbarter over 6 years ago

    Having started coding my LoraWan custom board using mbed I eventually switched over to CubeIDE.  The mbed environment is confusuing at times especially when creating a custom board for the first time.  It even kept switching my board type occassionally???    You do get a lot of code for free but it needs better documentation especially when creating a custom board.   And as mentioned above, you'll pull in more code than you need.

    My vote at this time (I really want mbed to succeed) is to go the CubeIDE route.  Add in a 6pin SWD connector and you can step through the code line by line in the debugger (I used a Tag-Connect cable. Saves a connector on the board).

    Other people may have better experience.  I've come from a Eclipse env (not great) for LynxOS and Visual Studio.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 6 years ago in reply to robbarter

    There will definitely be a debug connector (with the SWD pins), maybe even with the full ETM pins as well.

    (I'm still hoping someone will bring out a cheap debugger pod that supports it.)

     

    MK