• Products and Partners
    Products and Partners
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
Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Archaeology Resistivity Meter
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 332 replies
  • Subscribers 332 subscribers
  • Views 56326 views
  • Users 0 members are here
  • armp
  • archaeology resistivity meter
Related

Archaeology Resistivity Meter

kltm
kltm over 6 years ago

Hi I'm looking for ideas on an update to a resistivity meter for archaeology. The only published designs for diy were in 2 magazines. One was published in 1997 and the other in 2003. I have copies of both articles available. The reason behind this is the current high cost of available equipment, usually well beyond the reach of most archaeological groups. I've attached a basic block diagram. In the first magazine article the meter is very basic. It relied on the operators to write down the reading given as the survey was taken. Given that a normal survey grid is 20m x 20m and 1 reading is taken on every sq mtr there would be 400 readings to write down and then input into a program used to interpret the results. The later article is really an update to the first where a PIC has been added to record the readings. This again is prone to error, because eadings are taken manually by pressing a button.

I'm sure given the advances in electronics there must be better ways. 

 

 

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • kltm
    kltm over 6 years ago in reply to michaelkellett +8
    Hi Michael This all sounds very interesting and encouraging. I see you have found the original article, the update is also on slideshare somewhere. I haven’t really thought much about cost, but as you…
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz +7
    I can't live with that - I have to have symmetry The problem is that the Howland current pump doesn't constrain the voltage on the load at all when perfectly balanced - and my LTSpice model is unrealistically…
  • michaelkellett
    michaelkellett over 6 years ago in reply to michaelkellett +7
    AS promised - now for the phase sensitive detector. I couldn't easily model this in LTSpice, which is no great surprise because it needs multiplication and square roots. I used Simulink in MATLAB - which…
Parents
  • kltm
    kltm over 6 years ago

    Do we have a spec for proposed batteries and holders? I want to look at some form of easy removal without reverting to a screwdriver.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to kltm

    Hi Ken,

     

    It's a Sony design intended for cameras but many manufacturers produce it, so it is unlikely to go obsolete quickly. It is called Sony NP-F sized, there's a video about it here:

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    But any 7.4V LiPo ought to be fine, i.e. it is a decision the constructor can make. Some may already have (say) Canon or Nikon batteries so may prefer to use that. But personally I like the Sony design, it has large circular contacts, which feels more reliable for projects with low-cost battery holders.

     

    Also, maybe a small piece of foam is needed? since there could be shock or vibration, and double-check the lock on the battery-holder is sufficient or not. I don't have a mechanical background so I don't know what other precautions to take, however it could also be worth mounting the battery holder on some shock-absorbing material too.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 6 years ago in reply to kltm

    Hi Ken,

     

    It's a Sony design intended for cameras but many manufacturers produce it, so it is unlikely to go obsolete quickly. It is called Sony NP-F sized, there's a video about it here:

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    But any 7.4V LiPo ought to be fine, i.e. it is a decision the constructor can make. Some may already have (say) Canon or Nikon batteries so may prefer to use that. But personally I like the Sony design, it has large circular contacts, which feels more reliable for projects with low-cost battery holders.

     

    Also, maybe a small piece of foam is needed? since there could be shock or vibration, and double-check the lock on the battery-holder is sufficient or not. I don't have a mechanical background so I don't know what other precautions to take, however it could also be worth mounting the battery holder on some shock-absorbing material too.

    • Cancel
    • Vote Up +3 Vote Down