• Products and Partners
    Products and Partners
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
Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Archaeology Resistivity Meter
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 332 replies
  • Subscribers 332 subscribers
  • Views 56194 views
  • Users 0 members are here
  • armp
  • archaeology resistivity meter
Related

Archaeology Resistivity Meter

kltm
kltm over 6 years ago

Hi I'm looking for ideas on an update to a resistivity meter for archaeology. The only published designs for diy were in 2 magazines. One was published in 1997 and the other in 2003. I have copies of both articles available. The reason behind this is the current high cost of available equipment, usually well beyond the reach of most archaeological groups. I've attached a basic block diagram. In the first magazine article the meter is very basic. It relied on the operators to write down the reading given as the survey was taken. Given that a normal survey grid is 20m x 20m and 1 reading is taken on every sq mtr there would be 400 readings to write down and then input into a program used to interpret the results. The later article is really an update to the first where a PIC has been added to record the readings. This again is prone to error, because eadings are taken manually by pressing a button.

I'm sure given the advances in electronics there must be better ways. 

 

 

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • kltm
    kltm over 6 years ago in reply to michaelkellett +8
    Hi Michael This all sounds very interesting and encouraging. I see you have found the original article, the update is also on slideshare somewhere. I haven’t really thought much about cost, but as you…
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz +7
    I can't live with that - I have to have symmetry The problem is that the Howland current pump doesn't constrain the voltage on the load at all when perfectly balanced - and my LTSpice model is unrealistically…
  • michaelkellett
    michaelkellett over 6 years ago in reply to michaelkellett +7
    AS promised - now for the phase sensitive detector. I couldn't easily model this in LTSpice, which is no great surprise because it needs multiplication and square roots. I used Simulink in MATLAB - which…
Parents
  • kltm
    kltm over 6 years ago

    Great thank you.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to kltm

    Hello Ken,

    mk2 block diagram.

    Several changes,

    The DAC is driven by the FPGA

    The ADC has changed type to a TI single channel audio type (much cheaper (about £3.30) and OK for our purpose I think.)

    The ESP chip provides Bluetooth and WiFi, chosen because its widely available, dead cheap and there is a lot of app material on the web.

    The battery type is defined as Sony NP-F970 equivalent, 5AH gives about 35Whrs, and I estimate a WiFi and display on power

    consumption of 3W so the available batteries should give at least 10 hours per charge. I bought 2 and a charger for about £40.

    The display is ideally a Riverdi 4.3" which uses the Bridgetek controller and has SPI interface. You can get a bare bones one for about £36

    but the nice one with the touch screeen and flat glass front (like the PI display) is about £50. Or you can use a sub £5 quarter VGA type from

    China - but I won't be writing code for it image

     

    Any illegible and unguessable features, please ask.

     

    image

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to davemartin

    I have other instruments which make sensitive measurements, and (since I'm working on a desk and not in a field) I end up having to use rigid wire so that even the cabling doesn't move more than required to get the tests done. A movement or change in the bend of the wire causes a detectable difference for those types of measurements, partially because reactance changes.

    In the field, perhaps some of this can also be reduced, by (say) having an alert at the beginning to advise the user to verify the location of C1P1 is adequate and to use the specified wire technique (for instance not to loop the spare cable in your hand for part of the grid and not the rest of the grid), and so on, i.e. assist in training the user based on whatever best practices you have. Anyway, some of this can come later when the software or user procedures are documented by someone.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz

    Re. Sound,

     

    I did think about this a little while ago but forgot about it.

    The processor has an on chip DAC with good DMA control  - so we need to add a simple filter and power amplifier

    ( and a louspeaker) and we can make any sounds you can imagine.

    Perhaps Ken can add these to the block diagram.

     

    Re. Quality of connections to the ground and estimating such,

     

    The other point to bear in mind is that the processor is using it's 12 bit ADC to monitor the output voltage from the current source,

    so it can make a cycle by cycle (or even faster) assessment of how the current source is coping. To facilitate this there will need to be

    a digital signal from the FPGA to trigger the processors ADC. I always try to have a few uncommited signals available between

    FPGA and processor for when this sort of thing crops up.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to michaelkellett

    Hi kltm

     

    It will end up looking something like this on the block diagram:

    image

    Many thanks!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • kltm
    kltm over 6 years ago in reply to shabaz

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to kltm

    Great.

    I think I'm ready to draw up schematics.

    (You might think a formal spec should come first  - but we have a lot of stuff in this thread already and I find

    that trying to make a a complete design often helps focus on issues that abstract planning misses.

    Think of it as an Agile approach to hardware design image And schematics are easily changed.)

     

    I'm wondering if we should start new threads or make a new group for this project.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to michaelkellett

    Hi Michael,

    Hehe by random coincidence I was reading last night that it's a valid approach, to have elements of architecture and design co-occurring like you intuitively suggest! it's ISO 42020.

    Regarding group/thread I've never created a group on the platform so I'm unsure how it works but sounds like the right thing. Maybe Dudley or cstanton can advise the best method for such a project.

    Also, either way if a tag is also used (e.g. some unique codename/project name) and it is added to the new content and to this old thread, then it can be conveniently grouped up by Jive perhaps (like with a custom banner and intro etc, or at least just searchable based on that tag).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to shabaz

    Another option is to create a Document. It can be maintained by several people and has versioning.

    You can set who has edit right.

    Editing it is identical as with a blog post.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 6 years ago in reply to shabaz

    If there's a good reason for a group to be made then I can help that to happen.

    If the problem is trying to trawl through this entire thread, then there's an URL you can use which helps to display all of the comments, and that is Archaeology Resistivity Meter where ?displayFullThread=true is at the end of the URL.


    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • kltm
    kltm over 6 years ago in reply to cstanton

    Hi Christopher

     

    I would welcome your assistance in helping to set up a group for this project please.

     

    Ken

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 6 years ago in reply to kltm

    I need to know:

     

    - Who will administrate the group

    - Whether it should be publicly visible, or private

    - Depending on that, whether or not there is a list of people (links to their profiles or of their usernames are useful) who you want to be able to create content in the group, for example you might want a limited set of people to create discussions and blogs and documents, but only allow the public to comment on them.

    - If you have a preference for 'where' the group is listed or created on the site, which will be taken into consideration

     

    This can be sent in a private message.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • cstanton
    cstanton over 6 years ago in reply to kltm

    I need to know:

     

    - Who will administrate the group

    - Whether it should be publicly visible, or private

    - Depending on that, whether or not there is a list of people (links to their profiles or of their usernames are useful) who you want to be able to create content in the group, for example you might want a limited set of people to create discussions and blogs and documents, but only allow the public to comment on them.

    - If you have a preference for 'where' the group is listed or created on the site, which will be taken into consideration

     

    This can be sent in a private message.