• Products and Partners
    Products and Partners
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
Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Archaeology Resistivity Meter
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 332 replies
  • Subscribers 332 subscribers
  • Views 55982 views
  • Users 0 members are here
  • armp
  • archaeology resistivity meter
Related

Archaeology Resistivity Meter

kltm
kltm over 6 years ago

Hi I'm looking for ideas on an update to a resistivity meter for archaeology. The only published designs for diy were in 2 magazines. One was published in 1997 and the other in 2003. I have copies of both articles available. The reason behind this is the current high cost of available equipment, usually well beyond the reach of most archaeological groups. I've attached a basic block diagram. In the first magazine article the meter is very basic. It relied on the operators to write down the reading given as the survey was taken. Given that a normal survey grid is 20m x 20m and 1 reading is taken on every sq mtr there would be 400 readings to write down and then input into a program used to interpret the results. The later article is really an update to the first where a PIC has been added to record the readings. This again is prone to error, because eadings are taken manually by pressing a button.

I'm sure given the advances in electronics there must be better ways. 

 

 

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • kltm
    kltm over 6 years ago in reply to michaelkellett +8
    Hi Michael This all sounds very interesting and encouraging. I see you have found the original article, the update is also on slideshare somewhere. I haven’t really thought much about cost, but as you…
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz +7
    I can't live with that - I have to have symmetry The problem is that the Howland current pump doesn't constrain the voltage on the load at all when perfectly balanced - and my LTSpice model is unrealistically…
  • michaelkellett
    michaelkellett over 6 years ago in reply to michaelkellett +7
    AS promised - now for the phase sensitive detector. I couldn't easily model this in LTSpice, which is no great surprise because it needs multiplication and square roots. I used Simulink in MATLAB - which…
Parents
  • genebren
    genebren over 6 years ago

    Interesting ideas so far.  I meant to chime in earlier, but things have been pretty busy for me lately (building a deck and entertaining my Grandchildren again).

     

    Several years ago, I was asked to sit in with some friends of my sister that work at a geotech company.  They were looking to build impedance measurement devices for soil surveys.  I came across this amazing looking chip from Analog Devices that looked like a great way to measure impedance (including a complex component).

     

    Here is a snippet from the specification:

     

    The AD5934 is a high precision impedance converter system solution that combines an on-board frequency generator with a 12-bit, 250 kSPS, analog-to-digital converter (ADC). The frequency generator allows an external complex impedance to be excited with a known frequency. The response signal from the impedance is sampled by the on-board ADC and a discrete Fourier transform (DFT) is processed by an on-board DSP engine. The DFT algorithm returns a real (R) and imaginary (I) data-word at each output frequency.Once calibrated, the magnitude of the impedance and relative phase of the impedance at each frequency point along the sweep is easily calculated using the following two equations:Magnitude = 22IR+Phase = tan−1(I/R) A similar device, available from Analog Devices, Inc., is the AD5933, which is a 2.7 V to 5.5 V, 1 MSPS, 12-bit impedance converter, with an internal temperature sensor, available in a  16-lead SSOP.

     

     

    This might be of some help in your planning.

     

    Good luck and let me know if you need any help on this project.

     

     

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to genebren

    Hi Gene,

     

    It's a super-interesting chip, I was keen to use it a few years ago for plant soil purposes, and for hydroponics - to try to see if the soil or liquid has nutrients. The idea being to have a signature of known good soil or water by sweeping through the spectrum. I never got to try it though sadly, the project moved on to something else.

    It was felt that it could have had a lot of merit because then you could publish the signature, so others could try to replicate a yield (it wasn't going to be for farmers, more for home use), and to not waste nutrient. But, I have no idea in practice if the result would have been usable, or too inconsistent/variable.

    I wish I'd done some work on it at the time, since it could have been useful for other purposes too.

     

    The proposed design so far is one half of the impedance measuring system, but with digital processing. In theory it could be converted to an impedance measuring system with no additional hardware change, just a software upgrade, since the frequency will be know, and there will be some sync pulse from the FPGA, we just need to internally multiply with a 90 degree out of phase signal from that sync pulse too.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz

    I was thinking about generalising the design a bit - basically it's an impedance analyzer but with a restricted bandwidth and much higher than normal resolution.

    The chip that Gene mentions (AD5934) is let down by poor resolution (12 bit).

    The other big difference is that in the Earth resistance design we force current rather than the more common voltage.

    If we aim for 20mA RMS max current and 20VRMS excitation we can drive 400uA into 50k and 20mA into anything below 1k.

    The same system can be used for 4 wire resistance measurement, the 24 bit ADC,with gain at max of 64, should have noise and resolution

    well below 1uV, allowing us to resolve better than 50uOhms with 20mA excitation (possibly much better).

     

    I spent a little time doodling a +/-15V powered differential current source:

     

    image

     

    For 20mA 20V RMS operation R3 and R8 need to be 50R, 1VRMS drive needed on input. Op amps are LM7321 in SOIC package (to cope with the power).

     

    We would need to be able to monitor the voltage on the current amplifier outputs  to be sure it isn't limiting when driving into high impedance loads.

     

    NB:

     

    The circuit as simulated would not work with LM7321 due to its high bias and offset currents.

    In real life it would be better to use composite op amps for U1 and U2 where a high impedance low offset amp is buffered by a an LM7321 wired as a unity gain buffer.

     

    MK

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to michaelkellett

    Hi Michael,

     

    I had difficulty making it work too with a few different op amps, the output would look reduced for half of the waveform, and shifted down. I searched for ideas and found a doc (called "The differential Howland current source with high signal to noise ratio for bioimpedance measurement system", I can the PDF across) that suggests a 3-op-amp method, and that worked with the first op-amp I tried (OPA192). Then, I tried adding the LM7321:

    image

    I've not checked in detail, but the output looks good at birds-eye-view (the input VG is 100 Hz, 1Vpeak):

    image

    However, OPA192 is only rated for supplies up to +-18V. Also I don't know how bad the phase shift will be (since that will affect the measurement).

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz

    I can't live with that - I have to have symmetry image

     

    The problem is that the Howland current pump doesn't constrain the voltage on the load at all when perfectly balanced - and my LTSpice model is unrealistically perfect.

     

    I made a model in TINA (eeek what a revolting interface - I bought it once, a very long time ago - it a has neither changed nor improved.)

     

    This is a DC simulation of my model:

     

    image

     

    I did similar stuff in the LTSpice and it works there too.

    It might need a little more tuning but it's basically OK.

    R12 and R13 add a little tiny bit of voltage feedback, so slightly degrade the output impedance, but not by much.

    But they do fix the output voltage.

     

    I'll go on thinking about it, to see if I can come up with a better method.

    MK

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to michaelkellett

    Hi Michael,

    Oh, awesome. That in-a-row implementation was bugging me, I was concerned about the phase shift and the degradation. I'll try out this new iteration.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz

    Here's my first stab at the input amplifier. We need differential inputs that can take +/- 15V common mode  and outputs differential drive for the ADC centered on +2.5V.

    I can't do it without needing more power supplies - +7.5 and -2.5 for the ADC drive.

    Analog have the perfect chip, the LTC6373, does everything we want, but it's not actually released for production (and I've no idea of the price).

     

    This scheme will do, the traces in the simulation are the common mode signal from V8 and the two outputs. This is in x 0.25 mode, for x1 R3 and R4 become 1k,

    a relay will be needed to switch, the common mode range drops to about +/- 9V.

     

    If any one wants the LTSpice files for any of this stuff please ask.

     

    image

     

    V4 and V5 are driving the inputs at 100Hz. V8 is providing a big common mode voltage at 2 Hz.

     

    U1 and U2 need to rail to rail IO, low noise, low bias current, OPA192 will do, there are other cheaper options.

    R3,4,5 6 need to be 0.1% or better.

    I haven't drawn input protection but it will be needed.

     

    The power supply for this will be fun, +/-15V@30mA, +5V, +3.3V@200mA, +2.5V, + 7.5V, +1.2V, -2.5V.

     

     

    MK

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to michaelkellett

    The low current positive supply values may be a zener plus resisitor?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to michaelkellett

    Hi Michael,

    I had a stab at finding a solution to the power supplies.. I wasn't sure what source voltage to target, but I took an assumption of 6V, which could be two LiPo in series (e.g.  two 18650, or better still, a single camera battery, since they are low-cost, for hopefully at least a full day of use).

    I spent ages trying to find a transformer (and trying to shoe-horn stuff like audio transformers into the role unsuccessfully), but there's the 6-in-one coils, (all 1:1 ratio to each other) and two of those devices could provide enough windings to cover all the analog supply rails:

    Here the orange boxed windings are all one transformer, and the red boxed windings are the second transformer. The voltage regulator parts in the diagram are just placeholders, they don't represent any particular device.

    I'm wondering if something like LT3439 could drive them. Its also got a oscillator sync pin which could be useful.

    At 200 kHz I think VPH1-1400-RVPH1-1400-R (datasheet PDF) might be a suitable transformer. Regarding 5V, 3.3V and 1.2V, these could be from some DC-DC converter directly from the battery maybe. If you think this is the way to go, I can try to prototype up the analog supplies, since i'm not sure how effective I could simulate this.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to michaelkellett

    I just packed my house to move to Oregon yesterday and all my lab with it. So for the next few weeks I will mostly be working with computer, paper, and pencil only.

     

    michaelkellett - I am going to try to maintain LTspice by myself but will ask for your model if I get in trouble. There are a few things I don’t understand but let me try to work through them first.

    Regarding the following - I used to be a project manager. Forgive me image


    I think this string of comments will potentially become difficult to follow and it would be nice to see it well documented with up to date project description, diagrams, schematics, drawings, design files, etc. in one place. Is that best done on GitHub?  Anyway, I volunteer but request guidance. Do you have an opinion on using GitHub for project documentation other than just code Jan Cumps?  I am seeing this done quite a bit now.

    We should update the block diagram from shabaz early on. In my previous life the block diagram was fixed as well as key project objectives early in the project and only changed after much snarling and gnashing of teeth.  I propose the following be clarified now:

    * block diagram - key hardware like uC can be pencilled in for now, major things like whether to use a FPGA and architecture need to be fixed early

    * cost - 50£, 100£, 200£?  There should be some idea of single board cost.
    * component size and packages

    * the level of expertise required to build one - this will determine how many of these actually get built and used by DIYers.
    * Michael laid out a good summary of performance characteristics
    * I also like Michael’s comment that this could a general impedance analyzer. That is the way I would use it. The use cases need to be defined. Any others so as to minimize scope creep?

    Regarding the above I am happy to make something up to get it started but others may already know or have better thoughts.

     

    kltm do you have thoughts?  It would be great if other archaeologists found this useful and built one.
    Frank

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz

    Thanks for ideas.

    I like the idea of a standard dual lithium cell - can you point at any camera batteries ?

    I'm not thinking that hard about PSU yet, there's still a big Elephant in the shape of the display to resolve and it might use more power than everything else.

    However I would normally use some kind of switcher for the +/-15V supplies, LT8471 would do, LT3463 might do but is at the limit of power.

    The nice thing about using LT switchers is that they have models and example circuits in LTSpice.

    Some of the supplies will use very little current but must be low noise and I was thinking of using a quad op amp to tap down from the +/- 15 V supplies - not staggeringly efficient but low noise and simple.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz

    Thanks for ideas.

    I like the idea of a standard dual lithium cell - can you point at any camera batteries ?

    I'm not thinking that hard about PSU yet, there's still a big Elephant in the shape of the display to resolve and it might use more power than everything else.

    However I would normally use some kind of switcher for the +/-15V supplies, LT8471 would do, LT3463 might do but is at the limit of power.

    The nice thing about using LT switchers is that they have models and example circuits in LTSpice.

    Some of the supplies will use very little current but must be low noise and I was thinking of using a quad op amp to tap down from the +/- 15 V supplies - not staggeringly efficient but low noise and simple.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 6 years ago in reply to michaelkellett

    Hi Michael,

     

    The LT3439 is supposedly a low-noise driver which I'd thought I could prototype rapidly since I believed I had a dev-board for it and could have ripped out the transformer there, but turns out I have a different, LT3575 dev-board : ( I could knock up a test card on my next China PCB order and send one to you too if it's worthwhile just for general experimentation for any project, since we can't simulate that method well compared to the switcher designs.

    Sony NP-F series batteries seem quite good (original or some decent-mnfr third-party replacements), for instance this Amazon pack of two batteries and a charger is £30. The batteries come in different heights/capacities, all with the same footprint and attachment. I have a huge Ansmann brand 6.6Ah NP-F970 which fits my non-Sony camera monitor, so the range covers extremes and seems popular.

    There are NP-F holders on Aliexpress. Some chargers have adapter plates which are sold separately, so they are sometimes lower-cost.

    For a project recently, I used a cheaper adapter plate (about £10), and a smaller camera battery (not NP-F, I can't recall the model), and for that one I permanently fitted the adapter plate and battery inside the enclosure, because I put a charger circuit inside the box too. However for this use-case I guess that's not essential, and it could be an external mounted slide-on holder. Hehe I hope we're not speculating too much about how this project gets used! Still, it's more lightweight than lead-acid or whatever that the older systems may have run on : )

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz

    Hello Shabaz,

    I've not spotted the LT3439 before - there would be a big trade in efficiency against psu noise  - not sure yet that it's necessary for this project.

    Golly, that battery is £180 from Sony, I wonder what's inside the Amazon ones (ah - I see they only have half the capacity.)

    Plug in batteries are nice, or you could buy a 4 x 18650 pack with protection from RS, 7.4V @ 5.2 Ah about £30. But you wouldn't be able to swap charged up batteries in an emergency.

    If this box is to have a graphics display we need to scope its power requirement before we can really home in on a battery.

     

    Which leads to some questions I hope Ken can answer:

     

    Should the instrument have a graphics display ?

    Would the graphics only be useful if there was a full port of Snuffler or something like it ?

    I'm assuming it must have 10 hours endurance from a single charge - is that about right ?

    Is it worth the extra hassle (considerable in software) of being able to plug in either a USB stick or Micro SD card memory ?

     

    Some background information:

     

    A nice display (800 x 480, TFT colour capacitive touch) will add about £80 to the cost of the bits.

    USB card or SD card rather pushes you towards using an RTOS for the software and makes the software much more complicated.

    Running a big bit of code like Snuffler could be quite a lot of work.

    You can achieve these things by plugging into a laptop (has to be Windows for Snuffler so no RPi).

     

    MK

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to michaelkellett

    Hi Michael,

     

    I tried out the Snuffler software, and I feel it's definitely too much effort to replicate it, since it's not open source (but is free-to-use) and seems to be Windows-only. It does three main things:

     

    (1) accept data (either in real-time via COM port or from a flat file such as CSV), and the format is straightforward for at least one of the devices it works with,

    (2) plots the data,

    (3) graphically processes the data or manipulates it (for stuff like edge detection, interpolation and so on).

     

    For an on-board display, just speculating, perhaps only (1) and (2) could be needed, along with fewer basic graphic manipulation options, and as you say just use laptop if the full capabilities of (3) are needed. For on-board display to work I guess it does need to be a pretty nice display, since seeing the data is so core to it. I can try to investigate UART connected via USB to Android as an option (it is supported in Android Studio based apps apparently).. but depends if that's a usable practical scenario all day or if the built-in display is preferable.

     

    Also, incredible the price Sony is charging for what is still a consumer battery...

    The Ansmann 6.6 Ah battery is £35, it's a high-quality consumer brand too, so trustworthy I think. I have one of those batteries for about half a year, using this dual fast charger (£24). I don't have any Sony-manufactured gear that uses NP-F, but have ended up with a couple of items that can use the battery (a camera monitor, and a camera light both from different large brands (Atomos and Manfrotto) which optionally can have an adapter plate attached for NP-F, but the plate for the light is a separate purchased item which I don't own).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 6 years ago in reply to michaelkellett

    Michael,

     

    If it is desirable to support USB stick or Micro SD (with FAT support) there are a few options that will make the job a bit easier.

    1. There is this CH376 chip that handles the FAT structure and lets you write to USB Flash drives or SD cards (not too easy to find, as it does not seem to be handled by any common distributors - seems to only be available direct from the manufacturer).   There is a module available that is intended to interface with an Arduino that could be used ($12.95) from Marlin P. Jones Associates (https://www.mpja.com/USB-to-FAT-File-System-Control-Module-CH376-for-Arduino/productinfo/31813%20MP/)
    2. I have used something similar to this (Vinculum) to read/write USB drives (with FAT), the VINC2 parts can support SD cards).  It sure made it a lot easier to handle the task of file system support (and we were in a huge ARM part with tons of RAM).

     

    Good luck,

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to genebren

    Never seen those before !

    Not sure about reliability of supply and the data sheet is a bit lacking. Worth thinking about.

    The FTDI chips (Vinculum) might be be OK - I'll need to look again - I use their parts for USB serial ports on things quite a lot.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to michaelkellett

    These photos are not really related, except to show an adapter plate. My overall construction of this unit is poor, it was just a quickly-hacked-together low-noise low-current (100mA maximum I think) portable fixed-voltage DC supply project that I only needed for one use-case, but I'd like to re-do it properly sometime. The dual-Lithium battery here is a lot smaller than NP-F, about the size of a 9V PP3 battery:

    image

    The photo below shows the adapter plate (these are sold individually, normally used to fit the battery to a universal charger):

    image

    Final unit, just banana sockets, LED, power switch and I can charge it from 9-12V using the DC jack on the side:

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to shabaz

    Hi Shabaz,

    (1) and (2) in the Snuffler capabilities would seem easy to implement on a relatively low resolution screen In the field as you suggest. For a 20x20 or even 40x40 grid a simple graphic like heatmap in MATLAB could be displayed easily enough with a uC. That would allow an operator to see fliers or anomalies as they are appear.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to michaelkellett

    Good news, I searched around for a way to get USB UART with Android, and had some luck! I found some source code for MCP2221, and got it to eventually compile:

    image

    That's just the simulator, I need to test on my phone (I couldn't find my USB OTG cable, but I'll search for it later today, and then try it with a couple of baud rates to see what's supported!

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • kltm
    kltm over 6 years ago in reply to michaelkellett

    Hi a full graphics display wouldn’t be entirely necessary. It was done a few years back on a unit by T R SYSTEMS. They seem to have disappeared though. It was a box of electronics mounted on the side of the frame and an android tablet mounted facing the operator. The connection was remote and I guess Bluetooth. It’s complicated when surveying to work out exactly where you are on a grid, what with 20 rows to survey and 400 readings to take. Seeing numbers relating to your position is good, but it can still be confusing. We also have the added complication of obstructions, such as trees where we can take a reading. A dummy reading is taken in these instances. I’ve posted up my build of the original 2003 resistivity logger and there is also the GEOSCAN RM85 offering, both I feel overcomplicated in the number of buttons and very small displays. Equally the RM FROBISHER unit has a minimalist design, but a nightmare menu system behind it.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to kltm

    Here's my promised block diagram of how I see the story so far:

     

    image

     

    The bit you can't read on the right says that it could be a different display with an SPI interface.

    The Bridgetek thing I have in mind is an ME813A-WH50C (Farnell 2674200) but it is expensive - slightly cheaper from RS and similar things much cheaper from Mouser.

    I've used the Microchip BT module and I know it works, an ESP part might be preferred by some because it could do WiFi as well.

     

    I've put an SD card and USB OTG as options - they will need loads of software and probably a processor with more pins (than the 100 I've suggested).

     

    If we want to do much processing and have a big display on the board it might be better to go for a faster processor but it will use more power.

    I've suggested a low power version here.

     

    From comments so far it may be that a 4 line LCD character display would do for starters - it has the virtue of cheapness and simplicity.

    With care we could keep the interface dual purpose.

     

    I'm thinking of at least 8 Mbytes of directly connected and soldered in flash.

     

    Nothing is set in stone, additional scribbles and crossings out are welcomed.

     

    The basic idea of this design is that it uses sine wave excitation (lots of existing stuff uses square wave which is horrible).

    The phase sensitive detector is entirely in software.

    The FPGA is tiny (ICE40UP5) and costs about £5 - it is for glue purposes rather than computation.

    The proposed operator controls will be buttons and one or two rotary encoder type knobs.

    These go through the FPGA to avoid the use of high speed asynchronous interrupts that rotaries require (the FPGA is there so why not use it ?)

     

    Everything is software controlled - there are no hardware switches affecting filters, ranges, signal routing or stuff like that.

    The expansion interface could work a multiplexer (sometime far in the future).

     

    MK

    • Cancel
    • Vote Up +4 Vote Down