• Products and Partners
    Products and Partners
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
Open Source Hardware
  • Technologies
  • More
Open Source Hardware
Forum Archaeology Resistivity Meter
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Source Hardware to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 332 replies
  • Subscribers 332 subscribers
  • Views 56312 views
  • Users 0 members are here
  • armp
  • archaeology resistivity meter
Related

Archaeology Resistivity Meter

kltm
kltm over 6 years ago

Hi I'm looking for ideas on an update to a resistivity meter for archaeology. The only published designs for diy were in 2 magazines. One was published in 1997 and the other in 2003. I have copies of both articles available. The reason behind this is the current high cost of available equipment, usually well beyond the reach of most archaeological groups. I've attached a basic block diagram. In the first magazine article the meter is very basic. It relied on the operators to write down the reading given as the survey was taken. Given that a normal survey grid is 20m x 20m and 1 reading is taken on every sq mtr there would be 400 readings to write down and then input into a program used to interpret the results. The later article is really an update to the first where a PIC has been added to record the readings. This again is prone to error, because eadings are taken manually by pressing a button.

I'm sure given the advances in electronics there must be better ways. 

 

 

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • kltm
    kltm over 6 years ago in reply to michaelkellett +8
    Hi Michael This all sounds very interesting and encouraging. I see you have found the original article, the update is also on slideshare somewhere. I haven’t really thought much about cost, but as you…
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz +7
    I can't live with that - I have to have symmetry The problem is that the Howland current pump doesn't constrain the voltage on the load at all when perfectly balanced - and my LTSpice model is unrealistically…
  • michaelkellett
    michaelkellett over 6 years ago in reply to michaelkellett +7
    AS promised - now for the phase sensitive detector. I couldn't easily model this in LTSpice, which is no great surprise because it needs multiplication and square roots. I used Simulink in MATLAB - which…
Parents
  • kltm
    kltm over 6 years ago

    I usually use Camdenboss boxes. They have a screw on lid with a seal. They also have card slots in the side walls for mounting PCB’s. I would normally print the control panel and mount it under clear acrylic sheet.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to kltm

    Hello Ken,

     

    What do you think of this one:

     

    CHDX8-326, this is the ABS version so a very reasonable price of £17.35 for one or £14.38 each for five.

    We could put the display and main pcb in the lid and the batteries in the base.

    That way you would get a field openable box without any engineering work.

    Would still have to holes in the lid for the display and contols but that's inevitable.

     

    (Farnell sell the poly-carbonate version but not the ABS.)

     

    Did you have a different one in mind ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kltm
    kltm over 6 years ago in reply to michaelkellett

    Yes that box looks ok, just wondering if we would need to remove the batteries for charging. Is it possible to have a socket on the unit that you use for charging.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to kltm

    Hi Ken,

     

    I think that would be a major project (maybe better as a separate project to build a charger board that accepts a power supply with plug/socket). The camera batteries are better charged with off-the-shelf external chargers, they are not expensive, and they should be safe. Otherwise, fast charging such a large battery in a sealed enclosure will have heat implications, and could be risky. There's a few other reasons too, can elaborate if needed.

    Besides, the battery will take a long time to charge (3 hours or more) so swapping out the battery is quicker (dual external chargers exist).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz

    Certainly I think we should be able to remove the battery (or batteries), for the reasons Shabaz has suggested but also because if you run out in the field you need an instant fix.

    A charger could be added but I doubt if you would want it on the same board and it's quite a big project on it's own. I've designed a product with a single cell (1/6 of these camera things)

    and that took a lot of work to be sure of safety and performance.

     

    I've just discovered that no one seems to stock the ABS box (after I ordered the last one from Rapid image) but you can get the poly-carbonate one.

    I still like the idea because it gives you an openable box without a lot of work - but if we design the things sensibly people can pretty much

    use whatever box they like.

     

    I've just seen your box picture - what part number is that and how do you get it apart.- thanks.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kltm
    kltm over 6 years ago in reply to michaelkellett

    This box is CAMDENBOSS

    CRDCG0009CRDCG0009

     

    It's held together with 4 screws. If you look at it online it has a seal between the lid and the box. Seems Farnell no longer stock it, but CPC do. They have 8 in stock at £9.17 in 5's.

    Ken

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kltm
    kltm over 6 years ago in reply to michaelkellett

    This box is CAMDENBOSS

    CRDCG0009CRDCG0009

     

    It's held together with 4 screws. If you look at it online it has a seal between the lid and the box. Seems Farnell no longer stock it, but CPC do. They have 8 in stock at £9.17 in 5's.

    Ken

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • cstanton
    cstanton over 6 years ago in reply to kltm

    I made that a working product link for you.